mfgtool版本L4.1.15_2.0.0-ga_mfg-tools使用的是带rootfs目录下烧写。
IMX6ULL 使用官方的mfgtool烧写bsp报错,是什么原因呢?
which .vbs in the tools do you use? you can download the image to board successfully, but couldn't boo the board, right?
我这边使用的是 mfgtool2-yocto-mx-evk-sdcard-sd2.vbs 工具,
下载的BSP是L4.1.15_2.0.1-patch_images_MX6ULLEVK
I tested for you, I used mfgtool2-yocto-mx-evk-sdcard-sd1.vbs successfully, try to use this if yo use mx6ull evk board.
能加你的联系方式吗?
never-displayed