i.mx6ul mfg

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6ul mfg

647 Views
玉栋郭
Contributor III

hi everyone

 I'm trying download images use mfg,but I got error , what should i do ?

UTP: closing the file
UTP: sending Success to kernel for command frf.
utp_poll: pass returned.
UTP: received command 'pipe tar -jxv -C /mnt/mmcblkxp2/usr/local'
pid is 92, UTP: executing "tar -jxv -C /mnt/mmcblkxp2/usr/local"
UTP: sending Success to kernel for command pipe tar -jxv -C /mnt/mmcblkxp2/usr/local.
tar: can't change directory to '/mnt/mmcblkxp2/usr/local': No such file or directory
Kernel panic - not syncing: Attempted to kill init! exitcode=0x00008d00

g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage

Labels (2)
0 Kudos
1 Reply

384 Views
Yuri
NXP Employee
NXP Employee

Hello,

   please look at Getting started with Linux binary images on i.MX6UL EVK and MfgTool L3.14.52 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

 

0 Kudos