Dear team,
My customer is using i.MX6Q for their board and OS android 5.0.0
They using nfs booting but android immediately reboot
error 1
root@sabresd_6dq:/ # kill init: critical process 'servicemanager' exited 4 times in 4 minutes; rebooting into recovery mode
SysRq : Emergency Remount R/O
EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)
EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)
Emergency Remount complete
imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!
reboot: Restarting system with command 'recovery'
error 2
root@sabresd_6dq:/ # init: critical process 'healthd' exited 4 times in 4 minutes; rebooting into recovery mode
SysRq : Emergency Remount R/O
EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)
EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)
Emergency Remount complete
imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!
reboot: Restarting system with command 'recovery'
U-Boot 2014.04-00201-g9d7bf9b (May 04 2015 - 16:18:13)
What point do i check ?
Thanks, BR
Hi Allen kim,
It have many of reasons to facing this issue. Can you add entire bootlog and bootargs.
Thanks!
Aravinth
Hi Aleen
seems incorrect bootargs were used, please check parameter "nfsroot"
in attached Android_User's_Guide.pdf sect. 6.3.2 Kernel command line (bootargs)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------