Dear all,
I want to test USB OTG as storage device but I have some problem with adding kernel modules.
I currently use yocto with 3.14.52 version. Actually, I add g_mass_storage support as module but, it doesn't exist on kernel. Here is my log file.
root@imx6dlsabresd:~# insmod g_mass_storage.ko file=/dev/mmcblk1p1
insmod: can't insert 'g_mass_storage.ko': No such file or directory
root@imx6dlsabresd:~# uname -a
Linux imx6dlsabresd 3.14.52-1.1.1_ga+gdb1bcba #140 SMP PREEMPT Thu Jul 21 16:50:46 EEST 2016 armv7l GNU/Linux
root@imx6dlsabresd:~#
device tree:
/**
*usbotg settings
*/
&usbotg {
vbus-supply = <®_usb_otg_vbus>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usbotg>;
disable-over-current;
srp-disable;
hnp-disable;
adp-disable;
status = "okay";
dr_mode = "otg";
};
pin config:
Here are my kernel config about selection.
Best Regards,
Eren
Solved! Go to Solution.
I think you must run "bitbake core-image-minimal", so you miss "kernel" directory.
At least you should run "bitbake core-image-base".
I think you must run "bitbake core-image-minimal", so you miss "kernel" directory.
At least you should run "bitbake core-image-base".
Hi,
I understand that yocto generates modules.tar.gz separetly. I just refresh zImage and rootfs. Now the problem solved.
Thanks
That means no module installed default, so you should install modules manually.
modules in directory /lib/modules/3.14.28-1.0.0_ga+g91cf351/kernel
you can find "g_mass_storage.ko" in "/lib/modules/3.14.28-1.0.0_ga+g91cf351/kernel/drivers/usb/gadget"
root@imx6dlsabresd:/lib/modules/3.14.52-1.1.1_ga+gdb1bcba# ls
extra modules.builtin.bin modules.order
modules.alias modules.dep modules.softdep
modules.alias.bin modules.dep.bin modules.symbols
modules.builtin modules.devname modules.symbols.bin
There is no related kernel directory on my side. Kernel directory and kernel objects are missing. I don't know I have chosen all gadget as a module. I follow the referance manuel but, it seems that something is missing. What could be the reason that why kernel directory is missing on my system.
HI Eren
for usb tests one can look at imx-test package (folder ../test/mxc_usb_test)
http://patches.openembedded.org/patch/110753/
also please check attached Linux Manual Chapter 40
CHIPIDEA USB Driver
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
I followwed the docuement and now. The module exits but there is something strange. The module exist but, it can unloadable with modprobe.
root@imx6dlsabresd:~# find / -name g_mass_storage
/sys/module/g_mass_storage
root@imx6dlsabresd:~# modprobe g_mass_storage
modprobe: module g_mass_storage not found in modules.dep
root@imx6dlsabresd:~#
Best Regards,
Eren
As storage device, you can run commands as below,
insmod configfs.ko
insmod libcomposite.ko
insmod usb_f_mass_storage.ko
insmod gadgetfs.ko
insmod g_mass_storage.ko file=/dev/mmcblk1p1
run "lsmod" to list modules installed.
Actually, no kernel object shown. I selected the parameters which are written in I.MX6 Linux Referance Manuel-40.
root@imx6dlsabresd:~# lsmod
Tainted: G
galcore 225842 0 - Live 0x7f000000 (O)
root@imx6dlsabresd:~# ls /lib/modules/3.14.52-1.1.1_ga+gdb1bcba/
extra modules.builtin.bin modules.order
modules.alias modules.dep modules.softdep
modules.alias.bin modules.dep.bin modules.symbols
modules.builtin modules.devname modules.symbols.bin
root@imx6dlsabresd:~#
Also here is output of "zgrep -i usb /proc/config.gz" command.
CONFIG_IMX_HAVE_PLATFORM_FSL_USB2_UDC=y
# CONFIG_USB_SWITCH_FSA9480 is not set
# USB Network Adapters
# CONFIG_USB_CATC is not set
# CONFIG_USB_KAWETH is not set
CONFIG_USB_PEGASUS=m
CONFIG_USB_RTL8150=m
CONFIG_USB_RTL8152=m
CONFIG_USB_USBNET=m
CONFIG_USB_NET_AX8817X=m
CONFIG_USB_NET_AX88179_178A=m
CONFIG_USB_NET_CDCETHER=m
CONFIG_USB_NET_CDC_EEM=m
CONFIG_USB_NET_CDC_NCM=m
# CONFIG_USB_NET_HUAWEI_CDC_NCM is not set
# CONFIG_USB_NET_CDC_MBIM is not set
# CONFIG_USB_NET_DM9601 is not set
# CONFIG_USB_NET_SR9700 is not set
# CONFIG_USB_NET_SR9800 is not set
# CONFIG_USB_NET_SMSC75XX is not set
# CONFIG_USB_NET_SMSC95XX is not set
# CONFIG_USB_NET_GL620A is not set
CONFIG_USB_NET_NET1080=m
# CONFIG_USB_NET_PLUSB is not set
# CONFIG_USB_NET_MCS7830 is not set
# CONFIG_USB_NET_RNDIS_HOST is not set
CONFIG_USB_NET_CDC_SUBSET=m
# CONFIG_USB_ALI_M5632 is not set
# CONFIG_USB_AN2720 is not set
CONFIG_USB_BELKIN=y
CONFIG_USB_ARMLINUX=y
# CONFIG_USB_EPSON2888 is not set
# CONFIG_USB_KC2190 is not set
CONFIG_USB_NET_ZAURUS=m
# CONFIG_USB_NET_CX82310_ETH is not set
# CONFIG_USB_NET_KALMIA is not set
# CONFIG_USB_NET_QMI_WWAN is not set
# CONFIG_USB_NET_INT51X1 is not set
# CONFIG_USB_IPHETH is not set
# CONFIG_USB_SIERRA_NET is not set
# CONFIG_USB_VL600 is not set
# CONFIG_AT76C50X_USB is not set
# CONFIG_USB_ZD1201 is not set
# CONFIG_USB_NET_RNDIS_WLAN is not set
# CONFIG_TOUCHSCREEN_USB_COMPOSITE is not set
# CONFIG_I2C_TINY_USB is not set
# USB GPIO expanders:
# USB-based Watchdog Cards
# CONFIG_USBPCWATCHDOG is not set
# CONFIG_IR_MCEUSB is not set
# CONFIG_IR_TTUSBIR is not set
CONFIG_MEDIA_USB_SUPPORT=y
CONFIG_USB_VIDEO_CLASS=m
CONFIG_USB_VIDEO_CLASS_INPUT_EVDEV=y
CONFIG_USB_GSPCA=m
# CONFIG_USB_M5602 is not set
# CONFIG_USB_STV06XX is not set
# CONFIG_USB_GL860 is not set
# CONFIG_USB_GSPCA_BENQ is not set
# CONFIG_USB_GSPCA_CONEX is not set
# CONFIG_USB_GSPCA_CPIA1 is not set
# CONFIG_USB_GSPCA_ETOMS is not set
# CONFIG_USB_GSPCA_FINEPIX is not set
# CONFIG_USB_GSPCA_JEILINJ is not set
# CONFIG_USB_GSPCA_JL2005BCD is not set
# CONFIG_USB_GSPCA_KINECT is not set
# CONFIG_USB_GSPCA_KONICA is not set
# CONFIG_USB_GSPCA_MARS is not set
# CONFIG_USB_GSPCA_MR97310A is not set
# CONFIG_USB_GSPCA_NW80X is not set
# CONFIG_USB_GSPCA_OV519 is not set
# CONFIG_USB_GSPCA_OV534 is not set
# CONFIG_USB_GSPCA_OV534_9 is not set
# CONFIG_USB_GSPCA_PAC207 is not set
# CONFIG_USB_GSPCA_PAC7302 is not set
# CONFIG_USB_GSPCA_PAC7311 is not set
# CONFIG_USB_GSPCA_SE401 is not set
# CONFIG_USB_GSPCA_SN9C2028 is not set
# CONFIG_USB_GSPCA_SN9C20X is not set
# CONFIG_USB_GSPCA_SONIXB is not set
# CONFIG_USB_GSPCA_SONIXJ is not set
# CONFIG_USB_GSPCA_SPCA500 is not set
# CONFIG_USB_GSPCA_SPCA501 is not set
# CONFIG_USB_GSPCA_SPCA505 is not set
# CONFIG_USB_GSPCA_SPCA506 is not set
# CONFIG_USB_GSPCA_SPCA508 is not set
# CONFIG_USB_GSPCA_SPCA561 is not set
# CONFIG_USB_GSPCA_SPCA1528 is not set
# CONFIG_USB_GSPCA_SQ905 is not set
# CONFIG_USB_GSPCA_SQ905C is not set
# CONFIG_USB_GSPCA_SQ930X is not set
# CONFIG_USB_GSPCA_STK014 is not set
# CONFIG_USB_GSPCA_STK1135 is not set
# CONFIG_USB_GSPCA_STV0680 is not set
# CONFIG_USB_GSPCA_SUNPLUS is not set
# CONFIG_USB_GSPCA_T613 is not set
# CONFIG_USB_GSPCA_TOPRO is not set
# CONFIG_USB_GSPCA_TV8532 is not set
# CONFIG_USB_GSPCA_VC032X is not set
# CONFIG_USB_GSPCA_VICAM is not set
# CONFIG_USB_GSPCA_XIRLINK_CIT is not set
# CONFIG_USB_GSPCA_ZC3XX is not set
# CONFIG_USB_PWC is not set
# CONFIG_USB_ZR364XX is not set
# CONFIG_USB_STKWEBCAM is not set
# CONFIG_USB_S2255 is not set
# CONFIG_VIDEO_USBTV is not set
# Webcam, TV (analog/digital) USB devices
# CONFIG_USB_MR800 is not set
# CONFIG_USB_DSBR is not set
# CONFIG_USB_KEENE is not set
# CONFIG_USB_RAREMONO is not set
# CONFIG_USB_MA901 is not set
CONFIG_SND_USB=y
CONFIG_SND_USB_AUDIO=m
# CONFIG_SND_USB_UA101 is not set
# CONFIG_SND_USB_CAIAQ is not set
# CONFIG_SND_USB_6FIRE is not set
# CONFIG_SND_USB_HIFACE is not set
# USB HID support
CONFIG_USB_HID=y
# CONFIG_USB_HIDDEV is not set
CONFIG_USB_OHCI_LITTLE_ENDIAN=y
CONFIG_USB_SUPPORT=y
CONFIG_USB_COMMON=y
CONFIG_USB_ARCH_HAS_HCD=y
CONFIG_USB=y
# CONFIG_USB_DEBUG is not set
CONFIG_USB_ANNOUNCE_NEW_DEVICES=y
# Miscellaneous USB options
CONFIG_USB_DEFAULT_PERSIST=y
# CONFIG_USB_DYNAMIC_MINORS is not set
CONFIG_USB_OTG=y
CONFIG_USB_OTG_WHITELIST=y
# CONFIG_USB_OTG_BLACKLIST_HUB is not set
CONFIG_USB_OTG_FSM=y
# CONFIG_USB_MON is not set
# CONFIG_USB_WUSB_CBAF is not set
# USB Host Controller Drivers
# CONFIG_USB_C67X00_HCD is not set
CONFIG_USB_XHCI_HCD=m
CONFIG_USB_EHCI_HCD=m
CONFIG_USB_EHCI_ROOT_HUB_TT=y
CONFIG_USB_EHCI_TT_NEWSCHED=y
CONFIG_USB_FSL_MPH_DR_OF=m
CONFIG_USB_EHCI_MXC=m
# CONFIG_USB_EHCI_HCD_PLATFORM is not set
# CONFIG_USB_OXU210HP_HCD is not set
# CONFIG_USB_ISP116X_HCD is not set
# CONFIG_USB_ISP1760_HCD is not set
# CONFIG_USB_ISP1362_HCD is not set
# CONFIG_USB_FUSBH200_HCD is not set
# CONFIG_USB_FOTG210_HCD is not set
# CONFIG_USB_OHCI_HCD is not set
# CONFIG_USB_SL811_HCD is not set
# CONFIG_USB_R8A66597_HCD is not set
# CONFIG_USB_IMX21_HCD is not set
# CONFIG_USB_HCD_TEST_MODE is not set
# CONFIG_USB_RENESAS_USBHS is not set
# USB Device Class drivers
# CONFIG_USB_ACM is not set
# CONFIG_USB_PRINTER is not set
# CONFIG_USB_WDM is not set
# CONFIG_USB_TMC is not set
# NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may
# also be needed; see USB_STORAGE Help for more info
# CONFIG_USB_STORAGE is not set
# USB Imaging devices
# CONFIG_USB_MDC800 is not set
# CONFIG_USB_MICROTEK is not set
# CONFIG_USB_MUSB_HDRC is not set
# CONFIG_USB_DWC3 is not set
# CONFIG_USB_DWC2 is not set
CONFIG_USB_CHIPIDEA=m
# CONFIG_USB_CHIPIDEA_UDC is not set
# CONFIG_USB_CHIPIDEA_HOST is not set
# CONFIG_USB_CHIPIDEA_DEBUG is not set
# USB port drivers
CONFIG_USB_SERIAL=m
CONFIG_USB_SERIAL_GENERIC=y
# CONFIG_USB_SERIAL_SIMPLE is not set
# CONFIG_USB_SERIAL_AIRCABLE is not set
# CONFIG_USB_SERIAL_ARK3116 is not set
# CONFIG_USB_SERIAL_BELKIN is not set
# CONFIG_USB_SERIAL_CH341 is not set
# CONFIG_USB_SERIAL_WHITEHEAT is not set
# CONFIG_USB_SERIAL_DIGI_ACCELEPORT is not set
# CONFIG_USB_SERIAL_CP210X is not set
# CONFIG_USB_SERIAL_CYPRESS_M8 is not set
# CONFIG_USB_SERIAL_EMPEG is not set
CONFIG_USB_SERIAL_FTDI_SIO=m
# CONFIG_USB_SERIAL_VISOR is not set
# CONFIG_USB_SERIAL_IPAQ is not set
# CONFIG_USB_SERIAL_IR is not set
# CONFIG_USB_SERIAL_EDGEPORT is not set
# CONFIG_USB_SERIAL_EDGEPORT_TI is not set
# CONFIG_USB_SERIAL_F81232 is not set
# CONFIG_USB_SERIAL_GARMIN is not set
# CONFIG_USB_SERIAL_IPW is not set
# CONFIG_USB_SERIAL_IUU is not set
# CONFIG_USB_SERIAL_KEYSPAN_PDA is not set
# CONFIG_USB_SERIAL_KEYSPAN is not set
# CONFIG_USB_SERIAL_KLSI is not set
# CONFIG_USB_SERIAL_KOBIL_SCT is not set
# CONFIG_USB_SERIAL_MCT_U232 is not set
# CONFIG_USB_SERIAL_METRO is not set
# CONFIG_USB_SERIAL_MOS7720 is not set
# CONFIG_USB_SERIAL_MOS7840 is not set
# CONFIG_USB_SERIAL_MXUPORT is not set
# CONFIG_USB_SERIAL_NAVMAN is not set
# CONFIG_USB_SERIAL_PL2303 is not set
# CONFIG_USB_SERIAL_OTI6858 is not set
# CONFIG_USB_SERIAL_QCAUX is not set
# CONFIG_USB_SERIAL_QUALCOMM is not set
# CONFIG_USB_SERIAL_SPCP8X5 is not set
# CONFIG_USB_SERIAL_SAFE is not set
# CONFIG_USB_SERIAL_SIERRAWIRELESS is not set
# CONFIG_USB_SERIAL_SYMBOL is not set
# CONFIG_USB_SERIAL_TI is not set
# CONFIG_USB_SERIAL_CYBERJACK is not set
# CONFIG_USB_SERIAL_XIRCOM is not set
CONFIG_USB_SERIAL_WWAN=m
CONFIG_USB_SERIAL_OPTION=m
# CONFIG_USB_SERIAL_OMNINET is not set
# CONFIG_USB_SERIAL_OPTICON is not set
# CONFIG_USB_SERIAL_XSENS_MT is not set
# CONFIG_USB_SERIAL_WISHBONE is not set
# CONFIG_USB_SERIAL_ZTE is not set
# CONFIG_USB_SERIAL_SSU100 is not set
# CONFIG_USB_SERIAL_QT2 is not set
# CONFIG_USB_SERIAL_DEBUG is not set
# USB Miscellaneous drivers
# CONFIG_USB_EMI62 is not set
# CONFIG_USB_EMI26 is not set
# CONFIG_USB_ADUTUX is not set
# CONFIG_USB_SEVSEG is not set
# CONFIG_USB_RIO500 is not set
# CONFIG_USB_LEGOTOWER is not set
# CONFIG_USB_LCD is not set
# CONFIG_USB_LED is not set
# CONFIG_USB_CYPRESS_CY7C63 is not set
# CONFIG_USB_CYTHERM is not set
# CONFIG_USB_IDMOUSE is not set
# CONFIG_USB_FTDI_ELAN is not set
# CONFIG_USB_APPLEDISPLAY is not set
# CONFIG_USB_SISUSBVGA is not set
# CONFIG_USB_LD is not set
# CONFIG_USB_TRANCEVIBRATOR is not set
# CONFIG_USB_IOWARRIOR is not set
# CONFIG_USB_TEST is not set
CONFIG_USB_EHSET_TEST_FIXTURE=y
# CONFIG_USB_ISIGHTFW is not set
# CONFIG_USB_YUREX is not set
# CONFIG_USB_EZUSB_FX2 is not set
# CONFIG_USB_HSIC_USB3503 is not set
# USB Physical Layer drivers
CONFIG_USB_PHY=y
CONFIG_NOP_USB_XCEIV=y
# CONFIG_AM335X_PHY_USB is not set
# CONFIG_SAMSUNG_USB2PHY is not set
# CONFIG_SAMSUNG_USB3PHY is not set
# CONFIG_USB_GPIO_VBUS is not set
# CONFIG_USB_ISP1301 is not set
CONFIG_USB_MXS_PHY=m
# CONFIG_USB_RCAR_PHY is not set
# CONFIG_USB_ULPI is not set
CONFIG_USB_GADGET=m
CONFIG_USB_GADGET_DEBUG=y
CONFIG_USB_GADGET_VERBOSE=y
CONFIG_USB_GADGET_DEBUG_FILES=y
CONFIG_USB_GADGET_DEBUG_FS=y
CONFIG_USB_GADGET_VBUS_DRAW=2
CONFIG_USB_GADGET_STORAGE_NUM_BUFFERS=2
# USB Peripheral Controller
CONFIG_USB_FSL_USB2=m
# CONFIG_USB_FUSB300 is not set
# CONFIG_USB_FOTG210_UDC is not set
# CONFIG_USB_GR_UDC is not set
# CONFIG_USB_R8A66597 is not set
# CONFIG_USB_PXA27X is not set
# CONFIG_USB_S3C_HSOTG is not set
# CONFIG_USB_MV_UDC is not set
# CONFIG_USB_MV_U3D is not set
# CONFIG_USB_M66592 is not set
# CONFIG_USB_NET2272 is not set
# CONFIG_USB_DUMMY_HCD is not set
CONFIG_USB_LIBCOMPOSITE=m
CONFIG_USB_F_ACM=m
CONFIG_USB_F_SS_LB=m
CONFIG_USB_U_SERIAL=m
CONFIG_USB_U_ETHER=m
CONFIG_USB_F_SERIAL=m
CONFIG_USB_F_OBEX=m
CONFIG_USB_F_NCM=m
CONFIG_USB_F_ECM=m
CONFIG_USB_F_EEM=m
CONFIG_USB_F_SUBSET=m
CONFIG_USB_F_RNDIS=m
CONFIG_USB_F_MASS_STORAGE=m
CONFIG_USB_F_FS=m
CONFIG_USB_CONFIGFS=m
CONFIG_USB_CONFIGFS_SERIAL=y
CONFIG_USB_CONFIGFS_ACM=y
CONFIG_USB_CONFIGFS_OBEX=y
CONFIG_USB_CONFIGFS_NCM=y
CONFIG_USB_CONFIGFS_ECM=y
CONFIG_USB_CONFIGFS_ECM_SUBSET=y
CONFIG_USB_CONFIGFS_RNDIS=y
CONFIG_USB_CONFIGFS_EEM=y
CONFIG_USB_CONFIGFS_MASS_STORAGE=y
CONFIG_USB_CONFIGFS_F_LB_SS=y
CONFIG_USB_CONFIGFS_F_FS=y
CONFIG_USB_ZERO=m
CONFIG_USB_ZERO_HNPTEST=y
# CONFIG_USB_AUDIO is not set
# CONFIG_USB_ETH is not set
# CONFIG_USB_G_NCM is not set
# CONFIG_USB_GADGETFS is not set
CONFIG_USB_FUNCTIONFS=m
# CONFIG_USB_FUNCTIONFS_ETH is not set
# CONFIG_USB_FUNCTIONFS_RNDIS is not set
CONFIG_USB_FUNCTIONFS_GENERIC=y
CONFIG_USB_MASS_STORAGE=m
CONFIG_USB_G_SERIAL=m
# CONFIG_USB_MIDI_GADGET is not set
# CONFIG_USB_G_PRINTER is not set
# CONFIG_USB_CDC_COMPOSITE is not set
# CONFIG_USB_G_ACM_MS is not set
# CONFIG_USB_G_MULTI is not set
# CONFIG_USB_G_HID is not set
# CONFIG_USB_G_DBGP is not set
# CONFIG_USB_G_WEBCAM is not set
# CONFIG_USBIP_CORE is not set
# CONFIG_PRISM2_USB is not set
# CONFIG_LINE6_USB is not set
# CONFIG_USB_SERIAL_QUATECH2 is not set
# CONFIG_USB_ENESTORAGE is not set
# CONFIG_USB_MSI3101 is not set
# CONFIG_USB_SN9C102 is not set
# CONFIG_USB_WPAN_HCD is not set