Hi community,
Currently i'm working with i.mx6 sabredl development board. i followed nxp document IMXLXYOCTOUG and achieved to bootup with sd card. Board works well with default hannstar 10.1" . Now, i m trying to connect and operate 1920x720 LVDS display (datasheet is attached) with the sabre board. As i saw from schmatic files and datasheet of the display, i will need converter board to convert from 30pin LVDS to 60 pin LVDS (i will make the converter board).
So,it will be really appreciated to point me that which configurations i should make on yocto to work 1920x720 mitsubishi display ?
Thanks.
Samet
Hi samet
for new lvds lcd settings one can check:
https://community.nxp.com/thread/355690
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------