i.mx6Dual platform hung up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6Dual platform hung up

639件の閲覧回数
zc_tee
Contributor III

Dear all,

I saw the problem as the thread below:

https://community.nxp.com/message/446502 

Is it solved in kernel 3.0.101?

ラベル(2)
0 件の賞賛
1 返信

442件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tee

to avoid such errors recommended to move to latest bsps (kernels) described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

as since 3.0.35(101) many arm/gpu errata were fixed, which could produce such issues.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛