i.mx6 sabre sdp ramdisk root file system problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 sabre sdp ramdisk root file system problem

6,514 Views
jongjinyi
Contributor I

I'm working on imx6s sabre sdp and trying to boot with ramdisk root file system, but it's not working.

With i.mx51, ramdisk root file system boot was successful with almost same configuarion.

Could somebody tell me what I missed?

Here is what have i done.

1. kernel config.

at kernel menuconfig, i've selected following configuration

General setup > initial ram filesystem and ram disk support

--> CONFIG_BLK_DEV_INITRD=y, CONFIG_RD_GZIP=y

Device drivers > block devices > ram block device support

--> CONFIG_BLK_DEV_RAM=y, CONFIG_BLK_DEV_RAM_COUNT=16, CONFIG_BLK_DEV_RAM_SIZE=4096

2. ramdisk creation

I made ramdisk image with rootfs created by ltib

dd if=/dev/zero of=ramdisk bs=1k count=131072  ==> 128MB ramdisk
mkfs.ext2 ramdisk
mount -t ext2 -o loop ramdisk /mnt/rootfs
cp -a ./ltib/rootfs/* /mnt/rootfs
umount dir_ramdisk
gzip ramdisk  ==> which create ramdisk.gz

3. ramdisk deployment

I placed u-boot, uImage, ramdisk.gz on SD slot 3 SD card,

0~1M : u-boot area

1M~5M : kernel area

5M~55M : ramdisk.gz area

with the following commend on linux host computer. (sdcard is recognized as /dev/sdc in my linux host)

dd if=u-boot of=/dev/sdc bs=512 seek=2 skip=2 conv=fsync

dd if=uImage of=/dev/sdc bs=512 seek=2048 conv=fsync

dd if=ramdisk.gz of=/dev/sdc bs=512 seek=10240 conv=fsync

4. kernel cmdline configuration at u-boot command

the following is what I entered at u-boot command line.

set bootargs console=ttymxc0,115200 nosmp video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 ldb=sin1 ip=10.175.93.16 initrd=0x10c00000,50M root=/dev/ram0 ramdisk_size=131072

mmc dev 2

mmc read 0x10800000 0x800 0x2000  ==> read 4Mbyte from 1M offset. kernel

mmc read 0x10c00000 0x2800 0x19000 ==> read 50Mbyte from 5M offset, ramdisk.gz

bootm

and then, kernel booting halted with the following message

mmcblk1: mmc2:b02c SD04G 3.69 GiB

mmcblk1: p1

PHY: 1:01 - Link is Up - 100/Full

IP-Config: Guessing netmask 255.0.0.0

IP-Config: Complete:

     device=eth0, addr=10.175.93.16, mask=255.0.0.0, gw=255.255.255.255,

     host=10.175.93.16, domain=, nis-domain=(none),

     bootserver=255.255.255.255, rootserver=255.255.255.255, rootpath=

RAMDISK: Couldn't find valid RAM disk image starting at 0.

List of all partitions:

1f00            1024 mtdblock0  (driver?)

1f01            3072 mtdblock1  (driver?)

b300         7757824 mmcblk0  driver: mmcblk

b310            2048 mmcblk0boot1  (driver?)

b308            2048 mmcblk0boot0  (driver?)

b318         3872256 mmcblk1  driver: mmcblk

  b319         3814912 mmcblk1p1 00000000-0000-0000-0000-000000000000

No filesystem could mount root, tried:  ext3 ext2 ext4 cramfs vfat msdos

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)

[<8004a834>] (unwind_backtrace+0x0/0xf8) from [<8050c514>] (panic+0x74/0x18c)

[<8050c514>] (panic+0x74/0x18c) from [<80008dac>] (mount_block_root+0x1e0/0x224)

[<80008dac>] (mount_block_root+0x1e0/0x224) from [<80008fc4>] (mount_root+0xe8/0x108)

[<80008fc4>] (mount_root+0xe8/0x108) from [<80009148>] (prepare_namespace+0x164/0x1bc)

[<80009148>] (prepare_namespace+0x164/0x1bc) from [<80008a04>] (kernel_init+0x108/0x13c)

[<80008a04>] (kernel_init+0x108/0x13c) from [<80044aa4>] (kernel_thread_exit+0x0/0x8)

Labels (3)
Tags (3)
0 Kudos
Reply
5 Replies

1,643 Views
LeonardoSandova
Specialist I

there is a related issue on this thread

https://community.freescale.com/message/362688#362688

it may be worth trying the same first approach: placing the ramdisk on RAM and calling bootm with two parameters (kernel_address ramdisk_address)

0 Kudos
Reply

1,643 Views
jongjinyi
Contributor I

I tried the first approach from the link https://community.freescale.com/message/362688#362688

But it's not working in my case.

To make ramdisk image which can be recognized by u-boot, I used following command

mkimage -n 'Ramdisk' -A arm -O linux -T ramdisk -C gzip -a 0x10c00000 -e 0x10c00000 -d ramdisk.gz ramdisk.gz.uboot

And I removed initrd=0x10c00000,50M parameter from u-boot bootargs.

But it shows the same result.

Is there any recommanded option when using mkimage?

I checked rootfs.ext2.gz.uboot which was created by ltib, but it show 0x0 form load address and entry point.

mkimage -l rootfs.ext2.gz.uboot

Image Name:   uboot ext2 ramdisk rootfs

Created:      Tue Jan  7 13:37:21 2014

Image Type:   ARM Linux RAMDisk Image (gzip compressed)

Data Size:    6394243 Bytes = 6244.38 kB = 6.10 MB

Load Address: 0x00000000

Entry Point:  0x00000000

I think it doesn't make sense.

0 Kudos
Reply

1,643 Views
alexyang
NXP Employee
NXP Employee

Try to add 'keepinitrd' to kernel boot parameter on u-boot, please.

Basically Linux is finding initramfs for root file system as default on init process of Linux if you check CONFIG_BLK_DEV_INITRD on kernel menuconfig and initramfs differs to RAM disk.

So the init process frees the allocated RAM region for root file system if rootfs which is loaded to DRAM is not initramfs.

But The parameter 'keepinitrd' prevents to free RAM region as RAM filesystem on executing the init process even if the loaded RAMfs isn't initramfs.

I expect that 'keepinitrd' can resolve your error. Please try it.

- Alex Yang

0 Kudos
Reply

1,643 Views
LeonardoSandova
Specialist I

The manufacting tool has a XML file indicating the way to flash a particular board/profile, can you look at this file (or flash a demo image using it) to see how it handles? you can at least see the kernel command line with the correct address value.

Leo

0 Kudos
Reply

1,643 Views
jongjinyi
Contributor I

Thank you for your answer.

But calling bootm with two parameter will be working with ramdisk image processed by mkimage - u-boot tool.

Normally created ramdisk image - built on loop device and then gzipped - will not be recognized by u-boot.

I wonder why my approach is not working.

I checked every steps I have done several times, but I cannot find any mistake.

On the other CPU platform including i.mx51, I could successfully boot the system with ramdisk root file system by using same approach.

Is there any difference on imx6s linux kernel?

shouldn't ramdisk image be loaded at 0x10c00000?

In addition, there is new u-boot environment variable.

rd_loadaddr=(0x10800000+0x300000)

does it mean ramdisk load address?

if it means ramdisk load address, it should be 0x10800000+0x400000, because kernel size is 3.7MB.

How can I use this environment variable?

0 Kudos
Reply