Hi,
I'd like to use 1 or 2 additional uart on i.MX53 QSB that is (are) not the Debug Uart on Linux (Yocto)
am I obliged to use those on J13 (26-28-32-34) as it seems they are use elsewhere ?.
Solved! Go to Solution.
The real thing here is not Yocto specific as you have to prepare the patches to Kernel and U-Boot.
Once you have those done, you should make a customer/project specific layer and add a board for you. After that add overridies to Kernel and U-Boot applying your patches so it is maintainable in future releases.
Check at http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html
I think this gives you an idea.
As an example from my previous question : I'd choose J13 pins 26 & 28 for uart_Txd_mux & uart_rxd_mux : are they availabel right away to use from Yocto ?
It is not related to Yocto but your kernel. You'll need to change the MUX in the kernel/bootloader.
Otavio,does it relies to chap 4 in the System Development User’s Guide ?
As I never did such things I'm not sure to understand the main point of this tool as it save to xml.
The real thing here is not Yocto specific as you have to prepare the patches to Kernel and U-Boot.
Once you have those done, you should make a customer/project specific layer and add a board for you. After that add overridies to Kernel and U-Boot applying your patches so it is maintainable in future releases.
Check at http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html
I think this gives you an idea.
Thanks Otavio, now I understand that :
to have the i.MX53QSB using uart4 3 (or else) I have to modify kernel via kernel patch(es) .
Can anybody help me ? :
from the Development user's guide it seems that I need to use IOMUX to change the i.MX53 QSB to have additional UART on the board (p169). Did I get it cleary or I can use any UART (not app one for sure) right away form the J13 ?
I think you can enable support for the APP UART in the kernel config. It should work, no?
Hi Otavio,
can you precise what is the "App UART" on the board please ?
Right David, it is not available in the board.
In this case I think you'll really need to plug it in J13. But I think you'll also need to change the board file to enable it.
OtavioSalvador a écrit:
In this case I think you'll really need to plug it in J13. But I think you'll also need to change the board file to enable it.
Ok, I assume that this "board file" is about the I/O definition. Thanks.
Nevertheless, I'm really surprised that from all the 5 UARTs not anyone can be accessed easier.