i.mx287 NAND FLASH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx287 NAND FLASH

956件の閲覧回数
毅刘
Contributor I

My project is using i.mx287, it can boot from a 1Gbit NAND flash (MT29F1G08ABADA), but not boot from a 8Gbit NAND flash(MT29F8G08ABABAWP) , they all follow the ONFI NAND Flash Protocol, I don't know where is the problem, is the NAND page size, block size or other parameters? Can you give me some suggestions,or recommend me a 8Gbit NAND flash that the i.mx287 can boot from?

ラベル(1)
0 件の賞賛
1 返信

556件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Yes, actually there is a problem with the MT29F8G08ABABAWP, it should work (it writes but has a problem with UBI FS).

Here's a list of NANDs that work with the i.MX28 EVK:

"NAND01GW3",

  "K9F1F08",

  "TC58NVG0S3",

  "NAND02GW3",

  "HY27UF082G2M, HY27UG082G2M, HY27UG082G1M",

  "MT29F2G08",

  "K9F2G08U0M",

  "TC58NVG1S3",

  "HY27UH084G2M, HY27UG084G2M, HY27UH084G1M",

  "MT29F4G08",

  "TH58NVG2S3",

  "HY27UH088G2M",

  "NAND08GW3BxANx",

  "MT29F8G08FABWG",

  "MT29F16G08ABACA(2GB)",

  "TC58NVG1D4BFT00",

  "TH58NVG3D4xFT00",

  "TH58NVG4D4xFT00",

  "TC58NVG2D4BFT00",

  "K9G4G08U0M",

  "HY27UT084G2M, HY27UU088G5M",

  "NAND04GW3C2AN1E",

  "K9G8G08U0M, K9HAG08U1M",

  "HY27UV08AG5M",

  "Intel JS29F08G08AAMiB1 and Micron MT29F8G08MAA; "

  "Intel JS29F08G08CAMiB1 and Micron MT29F16G08QAA",

  "K9LAG08U0M K9HBG08U1M K9GAG08U0M",

  "Intel JS29F32G08FAMiB1 and Micron MT29F32G08TAA",

  "MT29F4G08",

  "JS29F08G08AAMiB2, JS29F08G08CAMiB2",

  "JS29F32G08FAMiB2",

  "HY27UW08CGFM",

  "MT29F8G08FABWG",

  "MT29F4G08AAA",

  "K9F4G08",

  "K9K8G08UXM, K9NBG08U5A, K9WAG08U1A",

  "K9WAG08UXM",

  "K9F2G08U0A",

  "K9F1F08",

  "K9GAG08U0M",

  "K9LBG08U0M (32Gb), K9HCG08U1M (64Gb), K9MDG08U5M (128Gb)",

  "H27UAG, H27UBG",

  "H27UCG",

  "H27U8G8T2B",

  "TC58NVG3D1DTG00",

  "TC58NVG4D1DTG00",

  "TH58NVG6D1DTG20",

  "JS29F16G08AAMC1, JS29F32G08CAMC1",

  "MT29F16G08MAA, MT29F32G08QAA",

  "MT29F64G08TAA (32Gb), MT29F32G08CBAAA (32Gb) MT29F64G08CFAAA (64Gb)",

  "MT29F128G08CJAAA",

  "JSF64G08FAMC1",

  "K9LBG08U0D",

  "K9GAG08U0D, K9LBG08U1D, K9HCG08U5D",

  "K9NCG08U5M",

  "TC58NVG5D2ELAM8 (4GB), TH58NVG6D2ELAM8 (8GB)",

  "TH58NVG7D2ELAM8",

  "K9GBG08U0M (4GB, 1CE); K9LCG08U1M (8GB, 2CE); K9HDG08U5M (16GB, 4CE)",

  "K9LCGD88X1M(8GB, 1CE); K9HDGD8X5M(8GB, 2CE); K9PFGD8X7M(16GB, 4CE)",

  "H27UAG8T2ATR (2GB, 1CE)",

  "H27UBG8T2M (4GB, 1CE), H27UCG8UDM (8GB, 2CE), H27UDG8VEM (16GB, 4CE)",

  "H27UEG8YEM (32GB, 4CE)",

  "MT29F32G08CBAAA (4GB, 1CE), MT29F64G08CFAAA (8GB, 2CE)",

  "MT29F128G08CJAAA (16GB, 2CE)",

  "MT29F16G08CBABA (2GB, 1CE)",

  "MT29F32G08CBABA (4GB, 1CE); "

  "MT29F64G08CEABA (8GB, 2CE); "

  "MT29F128G08CJABA (16GB, 2CE); "

  "MT29F128G08CKABA (16GB, 2CE); "

  "MT29F64G08CBAAA(8GB, 2CE) ",


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛