i.mx25 532mhz?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx25 532mhz?

Jump to solution
1,227 Views
PatrickLin
Contributor I

    Hi:
The FSL site below stated that mx25 can run up to 532mhz? It is true or just typo?

https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX251

Labels (1)
0 Kudos
Reply
1 Solution
1,056 Views
PatrickStilwell
NXP Employee
NXP Employee

Any of the ARM processors can be overclocked to take advantage of your particular use case.  However, the i.MX25 CPU spec is 400MHz.

On page 1 of the datasheet:

At the core of the i.MX25 is Freescale's fast,proven, power-efficient implementation of the

ARM926EJ-S core, with speeds of up to 400 MHz.


View solution in original post

0 Kudos
Reply
3 Replies
1,057 Views
PatrickStilwell
NXP Employee
NXP Employee

Any of the ARM processors can be overclocked to take advantage of your particular use case.  However, the i.MX25 CPU spec is 400MHz.

On page 1 of the datasheet:

At the core of the i.MX25 is Freescale's fast,proven, power-efficient implementation of the

ARM926EJ-S core, with speeds of up to 400 MHz.


0 Kudos
Reply
1,056 Views
Yuri
NXP Employee
NXP Employee

Strictly speaking the i.MX25  is qualified / tested for CPU frequencies up to 400 MHz.

0 Kudos
Reply
1,056 Views
Nouchi
Senior Contributor II

Hello,

It's seems that is possible to clock the core @532Mhz, but this ARM core only support 400MHz, it could work, .....or not

0 Kudos
Reply