hi everyone......
I am new to embedded...., presently working on imx53 QSB start-r.
Can anyone clarify what following macros actually return or what actually they mean....?
Macros are available in \kernel\arch\arm\plat-mxc\include\mach\iomux-mx53.h
.
I am using linaro build of ICS.
#define MX53_PAD_KEY_ROW0__UART4_RXD_MUX (_MX53_PAD_KEY_ROW0__UART4_RXD_MUX | MUX_PAD_CTRL(MX53_UART_PAD_CTRL))
and
#define MX53_PAD_CSI0_DAT13__UART4_RXD_MUX (_MX53_PAD_CSI0_DAT13__UART4_RXD_MUX | MUX_PAD_CTRL(MX53_UART_PAD_CTRL))
What is the actual difference in using these macros, in which context should each be used??
here I am also attaching iomux-mx53.h file....
Thanks...
Original Attachment has been moved to: iomux-mx53.h.zip
解決済! 解決策の投稿を見る。
Hello,Poorna,
Try to do following :
(1)Adjusting muxing sequence of UART4
static iomux_v3_cfg_t mx53_loco_pads[] = {
.....
/* CSI0 */
// MX53_PAD_CSI0_DAT13__IPU_CSI0_D_13,
MX53_PAD_CSI0_DAT14__IPU_CSI0_D_14,
MX53_PAD_CSI0_DAT15__IPU_CSI0_D_15,
// MX53_PAD_CSI0_DAT16__IPU_CSI0_D_16,
// MX53_PAD_CSI0_DAT17__IPU_CSI0_D_17,
MX53_PAD_CSI0_DAT18__IPU_CSI0_D_18,
MX53_PAD_CSI0_DAT19__IPU_CSI0_D_19,
MX53_PAD_CSI0_VSYNC__IPU_CSI0_VSYNC,
MX53_PAD_CSI0_MCLK__IPU_CSI0_HSYNC,
MX53_PAD_CSI0_PIXCLK__IPU_CSI0_PIXCLK,
/*UART4*/
MX53_PAD_CSI0_DAT12__UART4_TXD_MUX,
MX53_PAD_CSI0_DAT13__UART4_RXD_MUX,
MX53_PAD_CSI0_DAT17__UART4_CTS,
MX53_PAD_CSI0_DAT16__UART4_RTS,
.....
}
(2)Comment MX53_PAD_CSI0_DAT12__GPIO5_30
In funciton static void __init mx53_loco_board_init(void), CSI0_DAT12 pin has been muxed as GPIO5_30, You should consider how to comment it .
static void __init mx53_loco_board_init(void)
{
int i, ret;
iomux_v3_cfg_t mc34708_int = MX53_PAD_CSI0_DAT12__GPIO5_30;
...
if (board_is_mx53_loco_mc34708()) {
if (board_is_rev(IMX_BOARD_REV_2)) {/*Board RevA*/
mc34708_int = MX53_PAD_CSI0_DAT12__GPIO5_30;
mx53_loco_mc34708_irq = MX53_LOCO_MC34708_IRQ_REVA;
} else if (board_is_rev(IMX_BOARD_REV_4)) {/*Board RevB*/
mc34708_int = MX53_PAD_CSI0_DAT5__GPIO5_23;
mx53_loco_mc34708_irq = MX53_LOCO_MC34708_IRQ_REVB;
}
mxc_iomux_v3_setup_pad(mc34708_int);
ret = gpio_request(mx53_loco_mc34708_irq, "mc34708-int");
if (ret) {
printk(KERN_ERR"request mc34708-int error!!\n");
return;
....
}
Regards,
Weidong
Hello,Poorna,
The definitions of all signals muxing are in iomux-mx53.h file. For example:
>>#define MX53_PAD_KEY_ROW0__UART4_RXD_MUX (_MX53_PAD_KEY_ROW0__UART4_RXD_MUX | MUX_PAD_CTRL(MX53_UART_PAD_CTRL))
It means KEY_ROW0 pad is muxed as UART4_RXD signal.
>>#define MX53_PAD_CSI0_DAT13__UART4_RXD_MUX (_MX53_PAD_CSI0_DAT13__UART4_RXD_MUX | MUX_PAD_CTRL(MX53_UART_PAD_CTRL))
It means CSI0_DAT13 pad is muxed as UART4_RXD signal.
That's to say, One signal(such as UART4_RXD) in internal IP can be muxed out through different PADs. then which one you will use ? you can determine it according to your applicaion.
Regards,
Weidong
Thank you Weidong for your quick reply.
I have to work with UART4 pins for connecting the device which i need to work with. In order to enable UART4 I need to use cts,rts.tx.rx pins of uart4. In some cases we usually pull-up/pull-down some pins to enable UART, in IMX53 how can i enable and disable uart4 pins through programming. I will be grateful for your reply. I need to implement some functions to enable and disable UART4 on imx53.
Hello,Poorna,
Please tell me which CPU PADs you use to mux UART4_CTS,UART4_RTS,UART4_TXD,UART4_RXD On your schematic.
UART4_CTS---> ?
UART4_RTS--->?
UART4_TXD---> ?
UART4_RXD---> ?
"?" - means which CPU pads.
weidong
Hi Weidong,
One more help, how to do similar operation like pullup and puldown for UART4 in order to enable and disable UART4 ....
I am using ICS version of android from Linaro. I am using Software control. And if I wish to up a gpio pin like "MX53_PAD_CSI0_DAT14__GPIO6_0" do we have some functio/macro like set_gpio()??
Hello,Poorna,
The final reslease version of android BSP for i.MX53 is R10.4 , it is android 2.3.7 and linux kernel is 2.6.35. But R13.4.1 version, even there is android BSP for i.MX53, we didn't do complete test for this version.
weidong
Hi,
I am using Linaro ICS bsp with kernel 3.1.0, basically this release is for QSB board but we are using it on Start-r board. Is there any problem with respect to the PMIC and presently we don't worry about the power aspects.
We have commented "MX53_PAD_CSI0_DAT12__IPU_CSI0_D_12" in file board-mx53_loco.c, even after commenting cant we use this pin for UART4 ?
with reagrds
poorna t
Hello,Poorna,
Since you have muxed CSI0_DAT12 as CSI0_D_12, you can't mux it as "UART4_TXD". you should mux UART4_TXD via other pads. Such as KEY_COL0 pin (MX53_PAD_KEY_COL0__UART4_TXD_MUX).
weidong
hello Weidong,
Thanks, I have commented MX53_PAD_CSI0_DAT12__IPU_CSI0_D_12 line in file 'board-mx53_loco.c', still can't I use it for UART4. I am noway concerned about PMIC. Will pmic effect my operation?.
Can you Give me a brief on PMIC usage, or a way to completely disable it.
The other issue I am facing is Mouse isn't working with ICS build.
Thanks
- Poorna T
Hi,Poorna,
The board you are using is MX53QSB(DA9053+I.MX535) or MX53-START-R(MC34708+I.MX535) ?
weidong
Hello Weidong,
I am using MX53-START-R, as i have also mentioned this in my first post.
Thank You....
Hello,Poorna,
Try to do following :
(1)Adjusting muxing sequence of UART4
static iomux_v3_cfg_t mx53_loco_pads[] = {
.....
/* CSI0 */
// MX53_PAD_CSI0_DAT13__IPU_CSI0_D_13,
MX53_PAD_CSI0_DAT14__IPU_CSI0_D_14,
MX53_PAD_CSI0_DAT15__IPU_CSI0_D_15,
// MX53_PAD_CSI0_DAT16__IPU_CSI0_D_16,
// MX53_PAD_CSI0_DAT17__IPU_CSI0_D_17,
MX53_PAD_CSI0_DAT18__IPU_CSI0_D_18,
MX53_PAD_CSI0_DAT19__IPU_CSI0_D_19,
MX53_PAD_CSI0_VSYNC__IPU_CSI0_VSYNC,
MX53_PAD_CSI0_MCLK__IPU_CSI0_HSYNC,
MX53_PAD_CSI0_PIXCLK__IPU_CSI0_PIXCLK,
/*UART4*/
MX53_PAD_CSI0_DAT12__UART4_TXD_MUX,
MX53_PAD_CSI0_DAT13__UART4_RXD_MUX,
MX53_PAD_CSI0_DAT17__UART4_CTS,
MX53_PAD_CSI0_DAT16__UART4_RTS,
.....
}
(2)Comment MX53_PAD_CSI0_DAT12__GPIO5_30
In funciton static void __init mx53_loco_board_init(void), CSI0_DAT12 pin has been muxed as GPIO5_30, You should consider how to comment it .
static void __init mx53_loco_board_init(void)
{
int i, ret;
iomux_v3_cfg_t mc34708_int = MX53_PAD_CSI0_DAT12__GPIO5_30;
...
if (board_is_mx53_loco_mc34708()) {
if (board_is_rev(IMX_BOARD_REV_2)) {/*Board RevA*/
mc34708_int = MX53_PAD_CSI0_DAT12__GPIO5_30;
mx53_loco_mc34708_irq = MX53_LOCO_MC34708_IRQ_REVA;
} else if (board_is_rev(IMX_BOARD_REV_4)) {/*Board RevB*/
mc34708_int = MX53_PAD_CSI0_DAT5__GPIO5_23;
mx53_loco_mc34708_irq = MX53_LOCO_MC34708_IRQ_REVB;
}
mxc_iomux_v3_setup_pad(mc34708_int);
ret = gpio_request(mx53_loco_mc34708_irq, "mc34708-int");
if (ret) {
printk(KERN_ERR"request mc34708-int error!!\n");
return;
....
}
Regards,
Weidong
Hi,Poorna,
Can UART4 be used now ?
Regards,
Weidong
Hi Weidong,
Thankyou... now I am able to work with UART4 on imx53. As I am using ICS build I am facing some problems.
Hi Weidong,
I am using following pins
MX53_PAD_CSI0_DAT17__UART4_CTS
MX53_PAD_CSI0_DAT16__UART4_RTS
MX53_PAD_CSI0_DAT13__UART4_RXD_MUX
MX53_PAD_CSI0_DAT12__UART4_TXD_MUX
ThankYou.....
Regards
Poorna T
Hello,Poorna,
Open linux/arch/arm/mach-mx5/mx53_loco.c and add those pin definitions:
static iomux_v3_cfg_t mx53_loco_pads[] = {
.....
/* CSI0 */
// MX53_PAD_CSI0_DAT13__IPU_CSI0_D_13,
MX53_PAD_CSI0_DAT14__IPU_CSI0_D_14,
MX53_PAD_CSI0_DAT15__IPU_CSI0_D_15,
// MX53_PAD_CSI0_DAT16__IPU_CSI0_D_16,
// MX53_PAD_CSI0_DAT17__IPU_CSI0_D_17,
MX53_PAD_CSI0_DAT18__IPU_CSI0_D_18,
MX53_PAD_CSI0_DAT19__IPU_CSI0_D_19,
MX53_PAD_CSI0_VSYNC__IPU_CSI0_VSYNC,
MX53_PAD_CSI0_MCLK__IPU_CSI0_HSYNC,
MX53_PAD_CSI0_PIXCLK__IPU_CSI0_PIXCLK,
/*UART4*/
MX53_PAD_CSI0_DAT17__UART4_CTS,
MX53_PAD_CSI0_DAT16__UART4_RTS,
MX53_PAD_CSI0_DAT13__UART4_RXD_MUX,
MX53_PAD_CSI0_DAT12__UART4_TXD_MUX,
.....
}
But by default, CSI0_DAT12 is used for interrupt of pmic on MX53QSB, please check your board.
mc34708_int = MX53_PAD_CSI0_DAT12__GPIO5_30; //QSB-STAR-R board , PMIC is MC34708
da9052_csi0_d12 = MX53_PAD_CSI0_DAT12__IPU_CSI0_D_12;// QSB board. pmic is DA9053
So if you are using one of above 2 boards, CSI0_DAT12 pin probably can't be used.
In addition, you don't need to do any extra pull-up / pull-down for UART4. these have been done in muxing definitions.
you can try it .
Regards,
Weidong