Am I going mad??
I have the i.mx 28 and i.mx 51 development boards, neither allow access to the I/O except through the expansion board... I can see the expansion port connector but no reference to a connector part number or an expansion board??
Please accept our apologies, that the documentation it is not quite well explaining
the expansion board ; this option was made for the i.MX28EVK and for the i.MX51EVK.
You can see an image under the following link:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX51EVKJ
If you click in buy/specifications you can find and order the expansion board, which may
be connected to the J53 of the i.MX28EVK board.
Best regards
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi John
please check schematic on links below ( under section
"Printed Circuit Boards and Schematics-Schematics" )
i.MX28 Evaluation Kit|Freescale
i.MX53 Quick Start Board|Freescale
Regarding expansion board, please look at link below
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX51EVKJ
If you click in buy/specifications you can find and order the expansion board, which may
be connected to the J53 of the i.MX28EVK board.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------