i bikbake the imx-5.10.35-2.0.0 for my imx6q sabre board,but failed to use a mouse or keyboard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i bikbake the imx-5.10.35-2.0.0 for my imx6q sabre board,but failed to use a mouse or keyboard

Jump to solution
2,715 Views
steven_zhang
Contributor V

i bikbake the imx-5.10.35-2.0.0 for my imx6q sabre board,but failed to use a mouse or keyboard. I checked the kernel config ,the usb is disabled ,i enabled the usb , compiling and the kernel ,updated the SD card ,but the broblem is the same,

 how can i enable the usb and make the mouse and keyboard work.

0 Kudos
1 Solution
2,604 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I have tested the newest version BSP, and the usb otg work, it can connect to the mouse and keyboard. Here you need connect one usb otg line.

20210906.jpeg

I see the "usb usb1: USB disconnect, device number 1" in your log file.

Could you take the connection of your board?

 

View solution in original post

0 Kudos
15 Replies
2,690 Views
steven_zhang
Contributor V

i tested the 4.14..98 ,the mouse is not available,i thing the usb hardware would be broken,

0 Kudos
2,687 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

How did you connect to the mouse by the usb otg port?

0 Kudos
2,698 Views
steven_zhang
Contributor V

i will try the 4.9.88 image.

0 Kudos
2,712 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The usb otg host is support, when board boot up you can use the usb otg port to connect the mouse and keyboard.

Here have you tried the demo images , does it works?

0 Kudos
2,703 Views
steven_zhang
Contributor V

i tried the wic image downding from the nxp web ,the problem is the same ,i run the menu configuration of the kernel ,finding out the usb is not selected.  how can i enable the usb by configing the kernel.

 

0 Kudos
2,698 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you tried the earlier version BSP, did it work? As I do not have the i.MX6Q board in my hand can not test it for you.

0 Kudos
2,697 Views
steven_zhang
Contributor V

i will try the 4.9.88 image ,

2,694 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

OK, wait for you test result.

0 Kudos
2,638 Views
steven_zhang
Contributor V

my customer bought a new IMX6Qp-SEB to test the OTG OR HOST,

1,trdiedd to run the  pre-compiled  imx-image-full-imx6qpdlslolex.wic image ,getting the belows:

     failure to load boot.scr or boot/boot.scr

2,tried to complile the MX6Qp-SEB  image  by default setting, the otg or host is not selected : the usb-otg_vubs is disabling.

3,selected the otg in the kernel confugration,added the dr_mode="otg" ,after run the image,got the attached logs.

steven_zhang_0-1630545439180.png

 

 

0 Kudos
2,605 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I have tested the newest version BSP, and the usb otg work, it can connect to the mouse and keyboard. Here you need connect one usb otg line.

20210906.jpeg

I see the "usb usb1: USB disconnect, device number 1" in your log file.

Could you take the connection of your board?

 

0 Kudos
2,590 Views
steven_zhang
Contributor V

I bought a nwe otg cable, the mouse and the keyboard are both ok on the IMX6Q board.

2,572 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Steven,

Good news it works.

Wish you have a nice day

Best Regards

Rita

0 Kudos
2,608 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I have tested on my board use the old BSP, it works:

usb 2-1: USB disconnect, device number 2
usb 2-1: new low-speed USB device number 3 using ci_hdrc
usb 2-1: New USB device found, idVendor=413c, idProduct=301a
usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 2-1: Product: Dell MS116 USB Optical Mouse
usb 2-1: Manufacturer: PixArt
input: PixArt Dell MS116 USB Optical Mouse as /devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/usb2/2-1/2-1:1.0/0003:413C:301A.0002/input/input11
hid-generic 0003:413C:301A.0002: input,hidraw0: USB HID v1.11 Mouse [PixArt Dell MS116 USB Optical Mouse] on usb-ci_hdrc.0-1/input0

 

 

For the newest version I will test later

0 Kudos
2,616 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using for the i.MX6QP-SDB board?

0 Kudos
2,612 Views
steven_zhang
Contributor V

imx-5.10.35-2.0.0

0 Kudos