Hi,
To get HDMI working in linux kernel, do I need to enable HDMI while uboot compilation?
Is building uboot with HDMI by using below command is needed for HDMI to work in kernel?
"make SOC=iMX8M flash_hdmi_spl_uboot"
Or HDMI in kernel is independent of uboot?
Kindly reply.
Thanks in advance.
Regards,
Yashavantha
Hi Bio_TICFSL,
U mean to say "make SOC=iMX8M flash_hdmi_spl_uboot" command is not needed, instead can use "make SOC=iMX8M flash_spl_uboot" to create flash.bin?
Thanks and Regards,
Yashavantha
Hi Bharath,
In "sources/meta-fsl-bsp-release/imx/meta-bsp/conf/machine/imx8mqevk.conf" file
change like below.
--- IMXBOOT_TARGETS = "flash_evk flash_evk_no_hdmi"
+++ IMXBOOT_TARGETS = "flash_evk"
Regrads,
Yashavantha