Hi,
To get HDMI working in linux kernel, do I need to enable HDMI while uboot compilation?
Is building uboot with HDMI by using below command is needed for HDMI to work in kernel?
"make SOC=iMX8M flash_hdmi_spl_uboot"
Or HDMI in kernel is independent of uboot?
Kindly reply.
Thanks in advance.
Regards,
Yashavantha
Hello yashavantha,
The HDMI is independent of uboot you can enable on uboot or kernel, but in the BSP it is enable by default.
Regards
Hi Bio_TICFSL,
U mean to say "make SOC=iMX8M flash_hdmi_spl_uboot" command is not needed, instead can use "make SOC=iMX8M flash_spl_uboot" to create flash.bin?
Thanks and Regards,
Yashavantha
Hello Yashavantha,
Do you know how to configure yocto to use flash_spl_uboot instead of flash_hdmi_spl_uboot?
Thanks,
Bharat
Hi Bharath,
In "sources/meta-fsl-bsp-release/imx/meta-bsp/conf/machine/imx8mqevk.conf" file
change like below.
--- IMXBOOT_TARGETS = "flash_evk flash_evk_no_hdmi"
+++ IMXBOOT_TARGETS = "flash_evk"
Regrads,
Yashavantha
Yashavantha,
Thanks a lot and that helped
Regards,
Bharat
Hi Bio_TICFSL,
Any updates?
Thanks and Regards,
Yashavantha