Hi,
As in MCIMX6SLEVK, the crystal part number mentioned is "7V24000002", but could not find the exact description for the crystal. Please let me know the crystal description(Freq. Stability,Freq. Tolerance,Load Capacitance) considered for the SLEVK design.
An orderable part number for the same would be of much help.
Thanks.
Pankaj Rana
Hi Pankaj
for crystal one can also look at BOM file iMX6_SABRE_SDB_DESIGNFILES
and i.MX6 Crystal Drive Level (24 MHz) EB830
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov ,
This query is much related to the SoloLite processor and the Evaluation Board - MCIMX6SLEVK. In the design we can see that 24 MHz crystal along with 2 - 16uF capacitors.
The part number mentioned in the EVK BOM is 7V24000002 from TXC Corp.
The 7V series crystal is available in 3 variants with respect to the Load Capacitance - 8pF,12pF,18pF. Not sure which Crystal variant was used Freescale ! Please update.
Also please let me know the Stray Capacitance value considered.
Thanks.
-Pankaj Rana
I does not matter what you are using SoloLite or other i.MX6
Processors - 24Mhz crystal requirements are the same.
Stray capacitance is provided in crystal datasheet and it is different
for each crystal.