i.MXRT1170 Flexspi timings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MXRT1170 Flexspi timings

1,061件の閲覧回数
acremonini
Contributor II

Hi,

I'm having some trouble in understanding Flexspi timings as they are reported in the datasheet of the i'mxRT1170 (IMXRT1170AEC).

Looking at the output waveforms and timings in chapter 4.5.2.2.1, it looks like after a falling edge data is held at least 1ns but next data is valid after a maximum time of 1ns... how is this possible? Shouldn't be Tdvo(max) greater than Tdho(min) if they have the meaning represented in the waveforms?

 

acremonini_1-1656572392981.png

 

acremonini_0-1656572191742.png

Moreover, if I look at actual waveforms data seems to go down almost simultaneously with the falling edge of the clock and the 1ns hold time is not true.

acremonini_2-1656573262643.png

Can anybody explain to me this behaviour?

Thanks,

Antonio

0 件の賞賛
返信
6 返答(返信)

1,056件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Shouldn't be Tdvo(max) greater than Tdho(min) if they have the meaning represented in the waveforms?
-- Yes, your understanding is right, so I think the Tdvo (min) should be 1 ns, further it also should be less than the Tdho.
I'll contact the AE team to confirm soon and give feedback to you.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,027件の閲覧回数
acremonini
Contributor II

Hi,

do you have any news?

Thanks,

Antonio

0 件の賞賛
返信

973件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @acremonini ,
After confirming, the correct values are Tdvo(max) = 4ns and Tdho(min) = 2ns
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

タグ(1)
0 件の賞賛
返信

970件の閲覧回数
acremonini
Contributor II

Thank you Jeremy,

but there's still something I can't figure out: in the waveform I posted it looks like data edges are simultaneous with clock falling edges, so the hold time of 2ns doesn't seem to be true.

Can you confirm this?

Antonio

0 件の賞賛
返信

964件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
In my opinon, though it's a bit confusing, however, I don't find something obvious wrong.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,006件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Sorry for the reply late and I'll inform you ASAP if get any feedback.
And please find these files in the attachment.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信