Hello Experts,
I am working on i.mx93 rpmsg_lite_str_echo_rtos example code given in SDK_2_14_2_MIMX9352xxxxM.
Here my use case is that I am sending some periodic data (10,1,0,0) from i.mx93's cortex-M33 to cortex-A55 at every 10 second.
At Linux side in c application, I am able to read this data using /dev/ttyRPMSG30, but after some time I am not getting any data in my c application.
After Checking dmesg log I found below errors,
[ 310.280524] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: timeout waiting for a tx buffer
[ 310.300143] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: rpmsg_send failed: -512
below is code snippet of the modified function to send data from cortex-M33 on rpmsg
void app_task(void *param)
{
volatile uint32_t remote_addr;
void *rx_buf;
uint32_t len;
int32_t result;
void *tx_buf;
uint32_t size;
#ifdef MCMGR_USED
uint32_t startupData;
/* Get the startup data */
(void)MCMGR_GetStartupData(kMCMGR_Core1, &startupData);
my_rpmsg = rpmsg_lite_remote_init((void *)startupData, RPMSG_LITE_LINK_ID, RL_NO_FLAGS);
/* Signal the other core we are ready */
(void)MCMGR_SignalReady(kMCMGR_Core1);
#else
my_rpmsg = rpmsg_lite_remote_init((void *)RPMSG_LITE_SHMEM_BASE, RPMSG_LITE_LINK_ID, RL_NO_FLAGS);
#endif /* MCMGR_USED */
rpmsg_lite_wait_for_link_up(my_rpmsg, RL_BLOCK);
my_queue = rpmsg_queue_create(my_rpmsg);
my_ept = rpmsg_lite_create_ept(my_rpmsg, LOCAL_EPT_ADDR, rpmsg_queue_rx_cb, my_queue);
(void)rpmsg_ns_announce(my_rpmsg, my_ept, RPMSG_LITE_NS_ANNOUNCE_STRING, RL_NS_CREATE);
/* Get RPMsg rx buffer with message */
result = rpmsg_queue_recv_nocopy(my_rpmsg, my_queue, (uint32_t *)&remote_addr, (char **)&rx_buf, &len, RL_BLOCK);
if (result != 0)
{
assert(false);
}
/* Release held RPMsg rx buffer */
result = rpmsg_queue_nocopy_free(my_rpmsg, rx_buf);
if (result != 0)
{
assert(false);
}
for (;;)
{
if(rpmsg_send) // this flag will become true at every 10 second
{
rpmsg_send = 0;
// convert to string
len = snprintf(app_buf, sizeof(app_buf), "%d,%d,%d,%d\r\n", voltage, 0, 0, 0);
if(len>0 && len<sizeof(app_buf))
{
tx_buf = rpmsg_lite_alloc_tx_buffer(my_rpmsg, &size, RL_BLOCK);
assert(tx_buf);
memcpy(tx_buf, app_buf, len);
result = rpmsg_lite_send_nocopy(my_rpmsg, my_ept, remote_addr, tx_buf, len);
if (result != 0)
{
assert(false);
}
}
}
}
}
PS: However, My C application stops receiving data from /dev/ttyRPMSG30, still I am able to see data sent by cortex-M33 to cortex-A55 in dmesg logs.
[ 45.085653] rpmsg_tty_cb39 2c 30 2c 30 2c 30 0d 0a 9,0,0,0..
[ 55.085541] rpmsg_tty_cb39 2c 30 2c 30 2c 30 0d 0a 9,0,0,0..
[ 65.085425] rpmsg_tty_cb39 2c 30 2c 30 2c 30 0d 0a 9,0,0,0..
[ 75.085237] rpmsg_tty_cb39 2c 30 2c 30 2c 30 0d 0a 9,0,0,0..
[ 78.585719] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 80.728381] systemd-journald[183]: Time jumped backwards, rotating.
[ 85.085242] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 95.085240] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 105.085263] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 115.085799] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 125.085247] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 135.085248] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 140.678248] systemd-journald[183]: Time jumped backwards, rotating.
[ 145.085823] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 155.085275] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 165.085317] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 175.085237] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 185.085252] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 195.085239] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 200.676232] systemd-journald[183]: Time jumped backwards, rotating.
[ 205.085237] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 215.085240] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 225.085244] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 235.085269] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 245.085246] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 255.085242] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 260.672888] systemd-journald[183]: Time jumped backwards, rotating.
[ 265.085242] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 275.085243] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 285.085332] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 295.085242] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 305.085237] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 310.280524] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: timeout waiting for a tx buffer
[ 310.300143] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: rpmsg_send failed: -512
[ 315.085240] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 320.668282] systemd-journald[183]: Time jumped backwards, rotating.
[ 325.085250] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 325.359356] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: timeout waiting for a tx buffer
[ 325.372434] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: rpmsg_send failed: -512
[ 335.085252] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 340.431001] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: timeout waiting for a tx buffer
[ 340.456112] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: rpmsg_send failed: -512
[ 345.086076] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 355.085254] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 355.521789] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: timeout waiting for a tx buffer
[ 355.538391] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: rpmsg_send failed: -512
[ 365.085237] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
[ 370.628025] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: timeout waiting for a tx buffer
[ 370.641824] imx_rpmsg_tty virtio1.rpmsg-virtual-tty-channel.-1.30: rpmsg_send failed: -512
[ 375.085242] rpmsg_tty_cb36 2c 30 2c 30 2c 30 0d 0a 6,0,0,0..
So, Experts Here I am requesting to please look into this and give me some guidance.
Hi Salas,
Thanks for your reply,
1. Cortex M33 SDK version: SDK_2.14.2_MIMX9352xxxxM
2. Linux BSP version: i.MX Linux Yocto Project BSP 6.1.1_1.0.0 Release
Please find attached test program for cortex M33 to send rpmsg data and linux c++ app to receive rpmsg data.
P.S: what is my main problem is that my c++ application is able to receive data for some time but after certain period of time c++ application is not receiving any data from /dev/ttyRPMSG30, however I am able to see data sent from cortex-m33 in linux kernel dmesg logs.
Hello @NZP
I modified a little your code:
for (;;)
{
if(rpmsg_send)
{
rpmsg_send = 0;
// convert to string
len = snprintf(app_buf, sizeof(app_buf), "%d,%d,%d,%d\r\n", voltage++, 0, 0, 0);
if(len>0 && len<sizeof(app_buf))
{
/* Get tx buffer from RPMsg */
tx_buf = rpmsg_lite_alloc_tx_buffer(my_rpmsg, &size, RL_BLOCK);
assert(tx_buf);
/* Copy string to RPMsg tx buffer */
memcpy(tx_buf, app_buf, len);
result = rpmsg_lite_send_nocopy(my_rpmsg, my_ept, remote_addr, tx_buf, len);
if (result != 0)
{
assert(false);
}
result = rpmsg_queue_nocopy_free(my_rpmsg, tx_buf);
if (result != 0)
{
assert(false);
}
}
}
}
}
I added:
result = rpmsg_queue_nocopy_free(my_rpmsg, tx_buf);
if (result != 0)
{
assert(false);
}
To free the tx buffer, and now you should not have the timeout waiting for a tx buffer rpmsg log.
Logs from dmesg:
Logs from your Linux application:
I modified the voltage variable to increment each iteration.
I can confirm that the cortex M is sending messages to cortex A by the dmesg command, but sometimes trying to read form the ttyRPMSG30 the cortex A freeze for a moment, then work normally and It can read the ttyRPMSG30.
I am still investigating this issue.
Best regards.
Salas.
Thanks for reply.
I can confirm that the cortex M is sending messages to cortex A by the dmesg command, but sometimes trying to read form the ttyRPMSG30 the cortex A freeze for a moment, then work normally and It can read the ttyRPMSG30.
In my case once ttyRPMSG30 freezes it is not coming out. So, waiting for your observation.
Hi @Alejandro_Salas ,
After adding below at cortex-m33 side able to remove "timeout waiting for a tx buffer rpmsg log"
result = rpmsg_queue_nocopy_free(my_rpmsg, tx_buf); if (result != 0) { assert(false); }
but still getting the issue of freezing ttyRPMSG30.
Can you please suggest other strategy to debug this issue.