Hi,
I'm currently working on an i.MX8XQXP and I'm not able to find a definition of the shareability domains. From the A35 reference manual, I was able to find this information.
How were those signals set in the i.MX8X implementation? If the outer or inner shareability domain extend beyond the processor, which peripherals are included in each domain? Is there a specific documentation which provide this information ?
Kind Regards,
David
Hi David
one can look at
System Controller Firmware 101 - Resource management service
SCFW Porting Guide included in SCFW Porting Kit
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for the quick response. I looked at the link and I'm not sure if I understand completely. If the A35 cluster and a peripheral are in the same partition. How should I configure a MMU zone in the DDR for maximum efficiency? Would inner shareable be shared among all components of a partition ? Or would it be outer shareable.
Kind Regards,
David
Hi Igor,
Sure I wasn't really clear. For example, I'm working on the ENET and the buffer descriptor are written in DDR by the A35. If i set the MMU zone as cacheable outershareable. Would that configuration insure that a write by the A35 would be seen by the ENET? Or if I do a memory barrier DSB OSHST would that insure that the write is now visible to the ENET?
Kind Regards,
David
Hi Igor,
Thanks for the quick response. Would every peripherals see the write by the A35? If so, what is the difference between a memory barrier on outer shareable and one on the full system DSB ST for example. What about inner shareable would it only be seen between the cores inside the A35 cluster and no peripherals outside the cluster?
Kind Regards,
David
Hi David
>Would every peripherals see the write by the A35?
please look at suggested links in my first answer.
At references to resource : SC_R_A53, documentation gives expanations
which peripherals could be seen by A35 and how software configures it.
Regarding " memory barrier on outer shareable and one on the full system DSB ST" -
this applies to arm core operation. While "shareability domains" as far as I understood your
question refers to concept of " isolating resources from one another" - this is done
using SCU and SCFW : https://community.nxp.com/docs/DOC-341481
Best regards
igor