i.MX8QXP internal ring oscillator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8QXP internal ring oscillator

跳至解决方案
1,179 次查看
mamorukanou
Contributor IV

Hello, community

i.MX8QXP Reference Manual chapter 8.1 says:

This chapter describes the clocking for all the subsystems in the chip. The chip has three clock sources, two of them originate from external crystals and the third is generated internally by a ring oscillator. The two external crystal oscillators generate 24MHz and 32KHz, and the ring oscillator generates 200MHz. The 32KHz clock can be also sourced from an internal Ring Oscillator, but the frequency will be inaccurate ( +/- 20%) in this case.
The Ring Oscillator which can generate 200 MHz will be switched off after the initial start up and the 24MHz External Oscillator will take over for the remainder.

I have questions about this 200MHz clock.

Q1) This PLL is not written in the clock tree figure or table of the manual ?

Q2) Is this a provisional PLL until the DIG_PLL0 stabilizes after the power is turned on ?

  (During normal operation, this 200 MHz ring oscillator is not running.)

Best Regareds,

kanou

0 项奖励
回复
1 解答
1,117 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kanou

>Q1) This PLL is not written in the clock tree figure or table of the manual ?

right. Regarding its support please refer to below part of datasheet

pastedImage_1.jpg

>Q2) Is this a provisional PLL until the DIG_PLL0 stabilizes after the power is turned on ?

yes.

>During normal operation, this 200 MHz ring oscillator is not running.

right.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,118 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kanou

>Q1) This PLL is not written in the clock tree figure or table of the manual ?

right. Regarding its support please refer to below part of datasheet

pastedImage_1.jpg

>Q2) Is this a provisional PLL until the DIG_PLL0 stabilizes after the power is turned on ?

yes.

>During normal operation, this 200 MHz ring oscillator is not running.

right.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,117 次查看
mamorukanou
Contributor IV

Hi, Igor,

Thanks for your quick response.

I understood.

BR,

kanou

0 项奖励
回复