[ 1.424457] ehci-pci: EHCI PCI platform driver
[ 1.441283] ohci-pci: OHCI PCI platform driver
[ 2.809918] imx6q-pcie 5f010000.pcie: No cache used with register defaults set!
[ 2.845346] imx6q-pcie 5f010000.pcie: PCIe PLL is locked.
[ 2.860583] imx6q-pcie 5f010000.pcie: iATU unroll: disabled
[ 2.866237] imx6q-pcie 5f010000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[ 2.873907] imx6q-pcie 5f010000.pcie: host bridge /bus@5f000000/pcie@0x5f010000 ranges:
[ 2.889200] imx6q-pcie 5f010000.pcie: IO 0x007ff80000..0x007ff8ffff -> 0x0000000000
[ 2.905010] imx6q-pcie 5f010000.pcie: MEM 0x0070000000..0x007fefffff -> 0x0070000000
[ 2.921022] imx6q-pcie 5f010000.pcie: iATU unroll: disabled
[ 2.934114] imx6q-pcie 5f010000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[ 3.935037] imx6q-pcie 5f010000.pcie: Phy link never came up
[ 3.940769] imx6q-pcie 5f010000.pcie: PHY DEBUG_R0=0x00007e00 DEBUG_R1=0x08200000
[ 3.941390] imx6q-pcie: probe of 5f010000.pcie failed with error -110
PCIeb node in the device tree is mostly unchanged from the MEK - we've set a fixed lower link speed and a (currently unused) disable-gpio pin:
&pcieb{
compatible = "fsl,imx8qxp-pcie","snps,dw-pcie";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pcieb>;
pinctrl-1 = <&pinctrl_wifi_init>;
//disable-gpio = <&lsio_gpio1 3 GPIO_ACTIVE_LOW>;
reset-gpio = <&lsio_gpio4 0 GPIO_ACTIVE_LOW>;
clkreq-gpio = <&lsio_gpio4 1 GPIO_ACTIVE_LOW>;
ext_osc = <1>;
fsl,max-link-speed = <1>;
status = "okay";
};
pinctrl_wifi_init: wifi_initgrp{
fsl,pins = <
/* reserve pin init/idle_state to support multiple wlan cards */
IMX8QXP_SPI2_SCK_LSIO_GPIO1_IO03 0x06000021
>;
};
A notable difference is the VDD_PCIE_DIG_1P8_3P3 pin - we've set it to 1v8 in our custom board. However, the MEK board uses 3v3.
解決済! 解決策の投稿を見る。
Hello @riteshmpatel, thanks for the reply. We were able to correctly detect the external module after fixing a faulty differential PCB trace in our design.
Hello @riteshmpatel, thanks for the reply. We were able to correctly detect the external module after fixing a faulty differential PCB trace in our design.