i.MX8QXP+MAX9288

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8QXP+MAX9288

1,578件の閲覧回数
mdmosaddekhossa
Contributor II

Hallo NXP Team,

We have integrated GSML MAX9288 for video input for our custom i.MX8QXP board. We are using kernel version 4.19.98. Currently the driver is missing. I have not found the driver for this chip.

Can anyone provide me with the driver?

igorpadykov

Kind Regards,

Hossain

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,060件の閲覧回数
yuanke
Contributor I

i write driver for 9288,but when i test ,application blocked at DQBUF,is there someone can help me?

0 件の賞賛
返信

1,479件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hossain

one can use as reference max9286 driver, described in sect.6.1.7 V4L2 Capture

Linux 5.4.3_1.0.0 Documentation

max9286.c\imx8\platform\media\drivers - linux-imx - i.MX Linux kernel 

AR0144 and ov9284 drivers for I.MX8QM/QXP. | NXP Community 

for debugging one can try camera unit test:

mx8_v4l2_cap_drm.c\mxc_v4l2_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------