i.MX8QM MIPI-DSI Display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QM MIPI-DSI Display

389 Views
jars121
Contributor I

Hi,

I'm looking to use a 1920x1200 10-bit (8-bit with 2-bit FRC) panel with an i.MX8QM. The panel uses the MIPI-DSI interface; is this resolution and colour depth supported on the i.MX8QM MIPI-DSI at 60Hz (or perhaps 50Hz), or would I need to incorporate an HDMI bridge and instead use the i.MX8QM's HDMI output?

Thanks!

0 Kudos
Reply
1 Reply

371 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @jars121,

I hope you are doing well.

Please refer to Table 1. i.MX 8QuadMax advanced features of i.MX8QM datasheet.

Display controller supports single UltraHD 4Kp60 display or up to 4 independent FullHD 1080p60
displays.

Thanks & Regards,
Ritesh M Patel

 

0 Kudos
Reply