Hello,
I am using i.MX8MP processor with eMMC for persistent storage. I want to use secure boot (HAB) and create encrypted storage on eMMC using CAAM secure keys. eMMC is partitioned. I use one partition to store keys generated by caam-keygen and other partition (/dev/mmcblk2p7) is for the encrypted storage. I first created the encrypted storage on partition /dev/mmcblk2p7 using the steps descripted in AN12714. It works fine. I created a script that is called by Linux on my behalf at boot. The script imports key from blob, add it to the key retention service and mount the file system at /fsencrypted.
However, when I enabled HAB, I got the following errors at Linux boot.
<13>Jan 1 00:00:00 rc: Mounting enrypted storage on /dev/mmcblk2p7
[ 7.771096] caam_jr 30903000.jr: Failed to execute blob decap descriptor
[ 7.779322] caam_jr 30903000.jr: Blob decapsulation failed: -74
<13>Jan 1 00:00:00 rc:
<13>Jan 1 00:00:00 rc: CAAM keygen usage: caam-keygen [options]
<13>Jan 1 00:00:00 rc: Options:
<13>Jan 1 00:00:00 rc: create <key_name> <key_enc> <key_mode> <key_val> <text_type>
<13>Jan 1 00:00:00 rc: <key_name> the name of the file that will contain the black key.
<13>Jan 1 00:00:00 rc: A file with the same name, but with .bb extension, will contain the black blob.
<13>Jan 1 00:00:00 rc: <key_enc> can be ecb or ccm
<13>Jan 1 00:00:00 rc: <key_mode> can be -s or -t.
<13>Jan 1 00:00:00 rc: -s generate a black key from random with the size given in the next argument
<13>Jan 1 00:00:00 rc: -t generate a black key from a plaintext given in the next argument
<13>Jan 1 00:00:00 rc: <key_val> the size or the plaintext based on the previous argument (<key_mode>)
<13>Jan 1 00:00:00 rc: <text_type> can be -h or -p (default argument is -p)
<13>Jan 1 00:00:00 rc: -h generate a black key from the hex text that is provided in previous argument
<13>Jan 1 00:00:00 rc: -p generate a black key from the plain text that is provided in previous argument
<13>Jan 1 00:00:00 rc: import <blob_name> <key_name>
<13>Jan 1 00:00:00 rc: <blob_name> the absolute path of the file that contains the blob
<13>Jan 1 00:00:00 rc: <key_name> the name of the file that will contain the black key.
[ 7.915905] trusted_key: device-mapper: crypt: dm-0: INTEGRITY AEAD ERROR, sector 204672
[ 7.924042] trusted_key: device-mapper: crypt: dm-0: INTEGRITY AEAD ERROR, sector 204673
[ 7.932172] trusted_key: device-mapper: crypt: dm-0: INTEGRITY AEAD ERROR, sector 204674
[ 7.940292] trusted_key: device-mapper: crypt: dm-0: INTEGRITY AEAD ERROR, sector 204675
[ 7.948466] trusted_key: device-mapper: crypt: dm-0: INTEGRITY AEAD ERROR, sector 204676
[ 7.956639] trusted_key: device-mapper: crypt: dm-0: INTEGRITY AEAD ERROR, sector 204677
[ 7.964793] trusted_key: device-mapper: crypt: dm-0: INTEGRITY AEAD ERROR, sector 204678
[ 7.972971] trusted_key: device-mapper: crypt: dm-0: INTEGRITY AEAD ERROR, sector 204679
[ 7.982432] trusted_key: device-mapper: crypt: dm-0: INTEGRITY AEAD ERROR, sector 204672
[ 7.990562] trusted_key: device-mapper: crypt: dm-0: INTEGRITY AEAD ERROR, sector 204673
[ 7.998853] Buffer I/O error on dev dm-0, logical block 25584, async page read
[ 8.026440] EXT4-fs (dm-0): unable to read superblock
<13>Jan 1 00:00:00 rc: mount: /fsencrypted: can't read superblock on /dev/mapper/encrypted.
<13>Jan 1 00:00:00 rc: error: exit code 32
I figured out that I have to re-create the encrypted storage again (steps from AN12714) to get it working. However that removes my data stored on the partition.
To avoid these issues, seems I first have to enable HAB and then create encrypted storage.
My question is WHY? What happens with encrypted storage when I enable HAB? Do I do something wrong?
Thank you,
Jiri
解決済! 解決策の投稿を見る。
Thank you for explanation.