i.MX8MMini crop images before encoding with vpuenc_h264

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MMini crop images before encoding with vpuenc_h264

1,379 Views
vincentz63
Contributor IV

I need to crop the images acquired from a CSI sensor before encoding them with vpuenc_h264.

The doc states that the Hentro encoder (H1) has a pre-processing stage able to do cropping.

How do I use this block from GStreamer?

I have tried the following to no avail:

GST_DEBUG=3 gst-launch-1.0 videotestsrc ! video/x-raw,width=1920,height=1080,format=YUY2 ! videocrop top=0 left=0 right=1000 bottom=500 ! vpuenc_h264 ! fakesink
0:00:00.045524419 4163 0x146c7920 ERROR GST_PIPELINE grammar.y:740:gst_parse_perform_link: could not link videocrop0 to vpuenc_h264-0

Looking at the git repo, commit #056d64fe seems to indicate cropping is supported ("MMFMWK-8718 Enable cropping for hantro encoder at preprocess stage"). Is this correct?

I have also tried using imxvideoconvert_g2d as a workaround, but I have hit a problem. I am not sure if I am using the element properly or not, so any example would be appreciated.

Here is the pipeline I use for my test:

gst-launch-1.0 videotestsrc ! video/x-raw,width=1920,height=1080,format=YUY2 ! videocrop top=0 left=0 right=1856 bottom=1016 ! imxvideoconvert_g2d ! fakesink

So long as right<=1856 and bottom<=1016, the pipeline negotiates and seems to work. However, if I increase 'right' or 'bottom' by just 1 pixel, it fails to negotiate with the following error.

Any idea what I might be doing wrong? Am I using imxvideoconvert_g2d in the right way?

gstutils.c:2053:gst_element_link_pads_full: no link possible from videocrop0 to imxvideoconvert_g2d0
0:00:00.259336221 4136 0x38d63c00 INFO default gstutils.c:2162:gst_element_link_pads_filtered: Could not link pads: videocrop0:(null) - imxvideoconvert_g2d0:(null)
0:00:00.259358847 4136 0x38d63c00 ERROR GST_PIPELINE grammar.y:740:gst_parse_perform_link: could not link videocrop0 to imxvideoconvert_g2d0

 

More error output below

multiview-mode=(string){ mono, left, right }
0:00:00.259080463 4136 0x38d63c00 DEBUG GST_CAPS gstpad.c:2280:gst_pad_link_check_compatible_unlocked:<imxvideoconvert_g2d0:sink> sink caps video/x-raw, width=(int)[ 64, 2147483647 ], height=(int)[ 64, 2147483647 ], format=(string){ RGB16, RGBx, RGBA, BGRA, BGRx, BGR16, ARGB, ABGR, xRGB, xBGR, I420, NV12, UYVY, YUY2, YVYU, YV12, NV16, NV21 }; video/x-raw(memory:SystemMemory, meta:GstVideoOverlayComposition), width=(int)[ 64, 2147483647 ], height=(int)[ 64, 2147483647 ], format=(string){ RGB16, RGBx, RGBA, BGRA, BGRx, BGR16, ARGB, ABGR, xRGB, xBGR, I420, NV12, UYVY, YUY2, YVYU, YV12, NV16, NV21 }
0:00:00.259118714 4136 0x38d63c00 DEBUG GST_CAPS gstpad.c:2298:gst_pad_link_check_compatible_unlocked: caps are not compatible
0:00:00.259132715 4136 0x38d63c00 INFO GST_PADS gstpad.c:2434:gst_pad_link_prepare: caps are incompatible
0:00:00.259152590 4136 0x38d63c00 INFO GST_PADS gstpad.c:2529:gst_pad_link_full: link between videocrop0:src and imxvideoconvert_g2d0:sink failed: no common format
0:00:00.259199842 4136 0x38d63c00 DEBUG GST_BUS gstbus.c:316:gst_bus_post:<bus0> [msg 0x38eee090] posting on bus structure-change message: 0x38eee090, time 99:99:99.999999999, seq-num 11, element 'sink', GstMessageStructureChange, type=(GstStructureChangeType)GST_STRUCTURE_CHANGE_TYPE_PAD_LINK, owner=(GstElement)"\(GstVideoCrop\)\ videocrop0", busy=(boolean)false;
0:00:00.259222217 4136 0x38d63c00 DEBUG bin gstbin.c:3716:gst_bin_handle_message_func:<pipeline0> [msg 0x38eee090] handling child sink message of type structure-change
0:00:00.259244218 4136 0x38d63c00 DEBUG bin gstbin.c:958:bin_remove_messages:<imxvideoconvert_g2d0:sink> deleting message 0x38eee110 of type structure-change (types 0x00001000)
0:00:00.259266094 4136 0x38d63c00 DEBUG GST_BUS gstbus.c:351:gst_bus_post:<bus0> [msg 0x38eee090] dropped
0:00:00.259285344 4136 0x38d63c00 DEBUG GST_ELEMENT_PADS gstutils.c:1947:gst_element_link_pads_full: trying dest pad imxvideoconvert_g2d0:src
0:00:00.259299970 4136 0x38d63c00 DEBUG GST_ELEMENT_PADS gstutils.c:1999:gst_element_link_pads_full: we might have request pads on both sides, checking...
0:00:00.259317595 4136 0x38d63c00 DEBUG GST_ELEMENT_PADS gstutils.c:2053:gst_element_link_pads_full: no link possible from videocrop0 to imxvideoconvert_g2d0
0:00:00.259336221 4136 0x38d63c00 INFO default gstutils.c:2162:gst_element_link_pads_filtered: Could not link pads: videocrop0:(null) - imxvideoconvert_g2d0:(null)
0:00:00.259358847 4136 0x38d63c00 ERROR GST_PIPELINE grammar.y:740:gst_parse_perform_link: could not link videocrop0 to imxvideoconvert_g2d0
0:00:00.259407598 4136 0x38d63c00 INFO GST_PIPELINE grammar.y:652:gst_parse_perform_link: linking some pad of imxvideoconvert_g2d named imxvideoconvert_g2d0 to some pad of GstFakeSink named fakesink0 (0/0) with caps "(NULL)"
0:00:00.259428349 4136 0x38d63c00 INFO GST_ELEMENT_PADS gstutils.c:1774:gst_element_link_pads_full: trying to link element imxvideoconvert_g2d0:(any) to element fakesink0:(any)
0:00:00.259443474 4136 0x38d63c00 DEBUG GST_ELEMENT_PADS gstutils.c:1881:gst_element_link_pads_full: looping through allowed src and dest pads
0:00:00.259459725 4136 0x38d63c00 DEBUG GST_ELEMENT_PADS gstutils.c:1884:gst_element_link_pads_full: trying src pad imxvideoconvert_g2d0:sink
0:00:00.259475975 4136 0x38d63c00 DEBUG GST_ELEMENT_PADS gstutils.c:1884:gst_element_link_pads_full: trying src pad imxvideoconvert_g2d0:src
0:00:00.259493851 4136 0x38d63c00 DEBUG GST_ELEMENT_PADS gstutils.c:1105:gst_element_get_compatible_pad: finding pad in fakesink0 compatible with imxvideoconvert_g2d0:src
0:00:00.259517476 4136 0x38d63c00 INFO GST_PADS gstutils.c:1035:gst_pad_check_link: trying to link imxvideoconvert_g2d0:src and fakesink0:sink
0:00:00.259535602 4136 0x38d63c00 DEBUG GST_CAPS gstutils.c:3058:gst_pad_query_caps:<imxvideoconvert_g2d0:src> get pad caps with filter (NULL)
0:00:00.259553853 4136 0x38d63c00 DEBUG query gstquery.c:679:gst_query_new_custom: creating new query 0x38dfcde0 caps
0:00:00.259582978 4136 0x38d63c00 DEBUG GST_PADS gstpad.c:4053:gst_pad_query:<imxvideoconvert_g2d0:src> doing query 0x38dfcde0 (caps)
0:00:00.259601854 4136 0x38d63c00 DEBUG basetransform gstbasetransform.c:668:gst_base_transform_query_caps:<imxvideoconvert_g2d0:src> peer filter caps (NULL)

Tags (1)
0 Kudos
Reply
6 Replies

1,343 Views
vincentz63
Contributor IV

Hi Zhiming,

As I explained in my opening post, I want to use the H1 video encoder's cropping facility advertised in IMX8MMRM_Reference_Manual_REV2.pdf page 4806.

I have managed to use imxvideoconvert_g2d to crop the image, but using a GPU to crop when the encoder has this functionality built-in is a suboptimal workaround that increases power consumption and adds latency to the video pipeline.

Please re-read my last post where I explain that I have managed to crop the video using the H1 encoder, but the CPU usage shoots up to 60% on a dual core (1.5GHz) i.MX8MMini.

Could you please try to find information about the expected performance of the cropping facility of the H1 encoder? None of the NXP documents I have access to provide this information. Failing that, do you have an example or test I could run to check the expected performance?

Kind regards,

JP

0 Kudos
Reply

1,320 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @vincentz63 

 

I didn't find performance test file in internal

 

BR

Zhiming

0 Kudos
Reply

1,324 Views
vincentz63
Contributor IV

Hello,

Any hope of getting a more in-depth answer to my query?

Thanks,

JP

0 Kudos
Reply

1,363 Views
vincentz63
Contributor IV

Hello,

Thanks for the quick response, but I'm still not clear how to go about using the cropping block of the H1 encoder in the i.MX8MMini.

i.MX_Linux_User's_Guide.pdf does not mention cropping anywhere but cropping has been implemented in the GStreamer element (see below).  Are are you saying that this code does not work?

The IMX8MMRM_Reference_Manual_REV2.pdf states that the vpuenc_h264 has support for cropping on page 4806, figure 15-14 (VPH H1 Encoder Block Diagram). The Ref Manual does not provide any details about it. I have traced the code from the GStreamer element to the H1 driver, but the H1 encoder used in the i.MX8MMini is an IP sold by VeriSilicon, and I do not have access to its datasheet, so understanding the driver is very difficult. 

I have managed to crop the video using the following pipeline (I had previously mis-interpreted the properties of videocrop).

v4l2src ! video/x-raw,width=1920,height=1080,format=YUY2 ! videocrop top=0 left=0 right=128 bottom=0 ! vpuenc_h264 ! rtph264pay name=pay0

It does crop 128 pixels to the right of the image, but the CPU usage shoots-up to 60% on a dual core i.MX. This is unlikely to be the expected performance of a hardware pre-processing block. So I suspect the driver memcpies the input image. But without the H1 datasheet, I do not know what to expect... although cropping should be implemented using a stride when reading the data, so no memcpy should be needed...

Looking at the source code, I can see that the metadata set by videocrop is used by the vpuenc_h264 GStreamer element:

plugins/vpu/gstvpuenc.c line 1022:

cropmeta = gst_buffer_get_video_crop_meta (frame->input_buffer);
if (cropmeta) {
enc->open_param.nPicWidth = cropmeta->width;
enc->open_param.nPicHeight = cropmeta->height;
}

and then later, line 1143:

enc_enc_param.nPicWidth = enc->open_param.nPicWidth;
enc_enc_param.nPicHeight = enc->open_param.nPicHeight;

I have verified that the memory used to store the input image is physical continuous memory so no memcpy occurs in the gstvpuenc.c (line 1063).

I have  traced those settings all the way to the VeriSilicon driver files (h264encapi.h/c, encpreprocess.c) but I cannot see how the cropping is done there.

So could you please explain to me how can I use the cropping block of the encoder, either via GStreamer or by pointing me to an example demonstrating its usage?

Thanks,

JP

0 Kudos
Reply

1,351 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

You can see this issue to use g2d :https://gitlab.freedesktop.org/gstreamer/gst-plugins-good/-/issues/843

 

BR

Zhiming

0 Kudos
Reply

1,371 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

All supported operations of GST are located in 7.3 Multimedia use cases, i.MX_Linux_User's_Guide.pdf

 

BR

Zhiming

0 Kudos
Reply