i.MX8MM using DSI to HDMI converter (Audio Sync)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MM using DSI to HDMI converter (Audio Sync)

681 Views
EErdem
Contributor I

Hello, I am using a DSI to HDMI bridge to get HDMI output.

My bridge IC is different from EVKs and it has I2S input to provide audio data with video data over HDMI.

Q1: Is there any dedicated I2S pins to ensure Video and Audio Sync

Q2: If it is okey to use any of SAI pins how can I make sure that Video and Audio outputs are delivered within sync.

Labels (1)
0 Kudos
Reply
1 Reply

677 Views
igorpadykov
NXP Employee
NXP Employee

Hi EErdem

 

>Q1: Is there any dedicated I2S pins to ensure Video and Audio Sync

 

no

 

>Q2: If it is okey to use any of SAI pins how can I make sure that Video and Audio

>outputs are delivered within sync.

 

I believe any sai can be used, seems sync is provided by linux dai interface, may

useful to look at 

https://wiki.analog.com/resources/tools-software/linux-drivers/drm/adv7511#dai_configuration

 

Best regards
igor

0 Kudos
Reply