Hi everybody
i.MX8MM MIPI-CSI How many MegaPixel cameras can be supported?
Theoretically, each channel supports up to 1.5Gbps
But in Application Reference Chap 13.1.1.1, the maximum speed was only 5M pixels at 15fps, or 1080p60fps
1. So, Is 5Mpixel, 30fps not supported?
5M*30fps*16bit/pixel= 2.4Gbps (< 1.5Gbx4Lanes)
2. Can I connect i.MX8MM with 8M pixel, or 12M pixel camera?
In the case of 10bit / Pixel, how much frame rate if possible?
Please help,
HaRyanl
已解决! 转到解答。
the max bandwidth is up to 4lanes 6Gbps, for the resolution, you can refer to :
13.4.6.1 Image resolution
MIPI CSI Slave block needs the configuration of Image resolution to measure one line
length exactly and detect frame end. Vertical resolution register has 16bits (16’h0001 ~
16’hFFFF) Horizontal resolution register has 16bits (16’h0004 ~ 16’hFFFC).