i.MX8MM MIPI-CSI How many MegaPixel cameras can be supported?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MM MIPI-CSI How many MegaPixel cameras can be supported?

Jump to solution
3,255 Views
haryanl
Contributor IV

Hi everybody

i.MX8MM MIPI-CSI How many MegaPixel cameras can be supported?

Theoretically, each channel supports up to 1.5Gbps

But in Application Reference Chap 13.1.1.1, the maximum speed was only 5M pixels at 15fps, or 1080p60fps

1. So, Is 5Mpixel, 30fps not supported?

5M*30fps*16bit/pixel= 2.4Gbps (< 1.5Gbx4Lanes)

2. Can I connect i.MX8MM with 8M pixel, or 12M pixel camera?

In the case of 10bit / Pixel, how much frame rate if possible?

 

Please help,

HaRyanl

 

 

Tags (1)
0 Kudos
Reply
1 Solution
3,220 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
9 Replies
3,229 Views
haryanl
Contributor IV

In case I use YUV 8bit with 12Mpixel camera, can I use 30fps?

12Mpixel * 8bit * 30fps * 1.35 = 3.89Gbps (<6Gbps / 4Lanes)

1.35 is "blanking intervals"

0 Kudos
Reply
3,227 Views
joanxie
NXP TechSupport
NXP TechSupport

no, I don't think so

YUV422 over 8 bit = 2 cycles/pixel

so 12M* 20FPS*1.35*2*8BIT>6G, you can use YUV422 over 16 bit = 1 cycle/pixel

 

0 Kudos
Reply
3,223 Views
haryanl
Contributor IV

So can I use 15fps with 12M 8bit YUV case?

12M*8bit*15fps*2Cycles*1.35=3.89Gbps

Looking forward to your help

0 Kudos
Reply
3,221 Views
joanxie
NXP TechSupport
NXP TechSupport

yes on theory

0 Kudos
Reply
3,217 Views
haryanl
Contributor IV

So what is the maximum achievement that NXP has achieved on the EVK board?

How many Megapixels, and how many fps?

0 Kudos
Reply
3,190 Views
joanxie
NXP TechSupport
NXP TechSupport

the max bandwidth is up to 4lanes 6Gbps, for the resolution, you can refer to :

13.4.6.1 Image resolution
MIPI CSI Slave block needs the configuration of Image resolution to measure one line
length exactly and detect frame end. Vertical resolution register has 16bits (16’h0001 ~
16’hFFFF) Horizontal resolution register has 16bits (16’h0004 ~ 16’hFFFC).

0 Kudos
Reply
3,186 Views
haryanl
Contributor IV

Thank for your help

0 Kudos
Reply
3,245 Views
joanxie
NXP TechSupport
NXP TechSupport

what data format do you capture? 10bits raw data?

0 Kudos
Reply
3,238 Views
haryanl
Contributor IV

Hi Joanxie

We are considering connecting with Monochrome RGB 8/10/12bit Sensor

I have attached the datasheet of the 3 sensor types below, please refer to that

0 Kudos
Reply