i.MX8MM MIPI-CSI How many MegaPixel cameras can be supported?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8MM MIPI-CSI How many MegaPixel cameras can be supported?

跳至解决方案
2,750 次查看
haryanl
Contributor IV

Hi everybody

i.MX8MM MIPI-CSI How many MegaPixel cameras can be supported?

Theoretically, each channel supports up to 1.5Gbps

But in Application Reference Chap 13.1.1.1, the maximum speed was only 5M pixels at 15fps, or 1080p60fps

1. So, Is 5Mpixel, 30fps not supported?

5M*30fps*16bit/pixel= 2.4Gbps (< 1.5Gbx4Lanes)

2. Can I connect i.MX8MM with 8M pixel, or 12M pixel camera?

In the case of 10bit / Pixel, how much frame rate if possible?

 

Please help,

HaRyanl

 

 

标记 (1)
0 项奖励
1 解答
2,715 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
9 回复数
2,724 次查看
haryanl
Contributor IV

In case I use YUV 8bit with 12Mpixel camera, can I use 30fps?

12Mpixel * 8bit * 30fps * 1.35 = 3.89Gbps (<6Gbps / 4Lanes)

1.35 is "blanking intervals"

0 项奖励
2,722 次查看
joanxie
NXP TechSupport
NXP TechSupport

no, I don't think so

YUV422 over 8 bit = 2 cycles/pixel

so 12M* 20FPS*1.35*2*8BIT>6G, you can use YUV422 over 16 bit = 1 cycle/pixel

 

0 项奖励
2,718 次查看
haryanl
Contributor IV

So can I use 15fps with 12M 8bit YUV case?

12M*8bit*15fps*2Cycles*1.35=3.89Gbps

Looking forward to your help

0 项奖励
2,716 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes on theory

0 项奖励
2,712 次查看
haryanl
Contributor IV

So what is the maximum achievement that NXP has achieved on the EVK board?

How many Megapixels, and how many fps?

0 项奖励
2,685 次查看
joanxie
NXP TechSupport
NXP TechSupport

the max bandwidth is up to 4lanes 6Gbps, for the resolution, you can refer to :

13.4.6.1 Image resolution
MIPI CSI Slave block needs the configuration of Image resolution to measure one line
length exactly and detect frame end. Vertical resolution register has 16bits (16’h0001 ~
16’hFFFF) Horizontal resolution register has 16bits (16’h0004 ~ 16’hFFFC).

0 项奖励
2,681 次查看
haryanl
Contributor IV

Thank for your help

0 项奖励
2,740 次查看
joanxie
NXP TechSupport
NXP TechSupport

what data format do you capture? 10bits raw data?

0 项奖励
2,733 次查看
haryanl
Contributor IV

Hi Joanxie

We are considering connecting with Monochrome RGB 8/10/12bit Sensor

I have attached the datasheet of the 3 sensor types below, please refer to that

0 项奖励