i.MX8MM EVK Cannot find i2c devices once Android is started

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MM EVK Cannot find i2c devices once Android is started

1,211 Views
martindenion
Contributor II

I'm trying to use the GPIO expander of the i.MX8MM EVK board (OS android) from the user space.
From U-Boot, on the I2C-2 bus, I can find a device at address 20 but once Android has started, I cannot find any i2c device with i2cdetect.

From U-Boot:

u-boot=> i2c dev 0
Setting bus to 0
u-boot=> i2c probe
Valid chip addresses:  25
u-boot=> i2c dev 1
Setting bus to 1
u-boot=> i2c probe
Valid chip addresses:  00 14 50 52 72 73
u-boot=> i2c dev 2
Setting bus to 2
u-boot=> i2c probe
Valid chip addresses:  20

 

From userspace:

evk_8mm:/ # i2cdetect -y 0
i2cdetect: /dev/i2c-0: No such file or directory
evk_8mm:/ # i2cdetect -y 1
i2cdetect: /dev/i2c-1: No such file or directory
evk_8mm:/ # i2cdetect -y 2
i2cdetect: /dev/i2c-2: No such file or directory

 

0 Kudos
Reply
1 Reply

1,204 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 Kudos
Reply