i.MX8M series LPDDR4 Max Density

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M series LPDDR4 Max Density

678 Views
neilwinlee
NXP Employee
NXP Employee

What is the MAX density of LPDDR4 of i.MX8M? My understanding it can only perform up to 4GB.

Can it perform LPDDR4 8GB (expandable to 32GB)?

If it can perform LPDDR4 8GB, which are the i.MX8 series that able to propose?

Labels (1)
1 Reply

506 Views
Yuri
NXP Employee
NXP Employee

Hello,

   The max memory capacity, supported by i.MX8M is 4GB.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------