已解决! 转到解答。
@Tori-san
Hello,
I think using default settings in our BSP may be left as is.
The temperature settings in themselves are not the problem for thermal considerations:
the main problem is how to implement optimal power dissipation in system.
Regards,
Yuri.
Hi, I also have a similar question. I don't understand why the trip points would be the same for both IMX8MMCEC (0 to 95 Celsius) and IMX8MMIEC (-40 to 105 Celsius). If the temp sensor has a 10C accuracy, why does a 95C critical trip point work for IMX8MMCEC (0 to 95 Celsius)?
Thanks, Emma
@Tori-san
Hello,
The thermal parameters are application dependent. NXP settings in NXP Linux BSP
may be considered as base recommendations.
From NXP Linux description:
Thermal driver is a necessary driver for monitoring and protecting the SoC. The thermal driver monitors the SoC temperature in a certain frequency from an internal thermal sensor.
It defines two trip points: critical and passive. Cooling device will take actions to protect the SoC according to the different trip points that SoC has reached:
• When reaching critical point, cooling device will shut down the system.
• When reaching passive point, cooling device will lower CPU frequency and notify GPU/VPU to run at a lower frequency.
• When the temperature drops to 10 °C below passive point, cooling device will release all the cooling actions.
Thermal driver has two parts:
• Thermal zone defines trip points and monitors the SoC's temperature.
• Cooling device takes the actions according to the different trip points.
Regards,
Yuri.
Hi Yuri,
Thank you for your reply.
Base recommendations are as follows in imx8mm.dtsi.
-------------------------------
trips {
cpu_alert0: trip0 {
temperature = <85000>;
hysteresis = <2000>;
type = "passive";
};
cpu_crit0: trip1 {
temperature = <95000>;
hysteresis = <2000>;
type = "critical";
};
};
-------------------------------
Would you recommend the following changes to the IMX8MMIEC (-40C to 105C)?
Is this changes at my own risk?
-------------------------------
trips {
cpu_alert0: trip0 {
temperature = <95000>;
hysteresis = <2000>;
type = "passive";
};
cpu_crit0: trip1 {
temperature = <105000>;
hysteresis = <2000>;
type = "critical";
};
};
-------------------------------
Best regards,
Tori-san.
@Tori-san
Hello,
I think using default settings in our BSP may be left as is.
The temperature settings in themselves are not the problem for thermal considerations:
the main problem is how to implement optimal power dissipation in system.
Regards,
Yuri.