i.MX8M mini TMU calibration method

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M mini TMU calibration method

Jump to solution
1,029 Views
Tori-san
Contributor III
Hello, According to the IMX8MMRM.pdf clause 5.4.6, hardware will do 1 point calibration (software can do 2 points calibration). So, is it possible to calibrate the temperature with both HW / SW? In that case, how to enable each HW / SW calibration? How to check which one is currently valid calibration method?
0 Kudos
1 Solution
1,008 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
3 Replies
974 Views
Tori-san
Contributor III

Hi Yuri,

Thank you for your reply.

I interpret that HW 1-point calibration is enabled by default and it using slope=1 as the equation.

Therefore, in case of HW, following is used for 1-point calibration, and the offset at 85C is not an issue.

 

Tcalib_HW = 1*(Tsense - TE1) + 25

 

Best regards,

Tori-san.

0 Kudos
1,009 Views
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  I've sent You some comments directly regarding

https://community.nxp.com/t5/i-MX-Processors/i-MX8M-mini-TMU-2-points-DC-offset-value-confirmation/m...

 

Regards,
Yuri.

 

0 Kudos
992 Views
Tori-san
Contributor III
Hi Yuri, I appreciate your reply for questions I posted. The question has become almost clear and I sent some comment as reply directly.