i.MX8M can't show analog camera frame correctly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8M can't show analog camera frame correctly

1,479 次查看
bensonhuang
Contributor III

Hi,

Our platform: i.MX8M

Video decoder: ISL79987

Analog camera: 2 camera 2 lane

Field: V4L2_FIELD_INTERLACED (NTSC)

Command: yavta -fUYVY -s720x480 -t1/30 --field seq-tb -n4 -c -F /dev/video0

      RAW Pixels  (1440x480) (left top is first camera top part, right top is second camera bottom part, left down is first camera bottom part, right down is second camera top part)

pastedImage_1.png

      RAW Pixels  (720x480) (left top and right top mix together, left down and right down mix together)

pastedImage_2.png

We have the following questions.

1. We capture 720x480 frame but it seems each captured frame is 720x240. Odd field and even field are all 720x120.

    Why can't we get 720x240 odd and even field?

2. The captured frame order is camera 1 -> camera 2 -> camera 1 -> camera 2.

    Could we get channel 1 (camera 1) total frame and then get channel 2 (camera 2) total frame?

    How could we ensure the order is correct?

3. What is the black bar between the frames? Could we have some way to remove it?

4. Our video source is NTSC. Bottom part is transmitted first and then top part.

    In yavta, do we need to use interlaced-bt for field setting?

5. If the deinterlace function works, what is the expected frame behavior?

    For 720x480 frame, the top part is channel 1 (camera 1) preview and the bottom part is channel 2 (camera 2) preview?

6. Are there any other tools for verifying the captured frame except yavta?

Thanks.

4 回复数

246 次查看
cbl
Contributor IV

Hello @bensonhuang,

I am developing on the i.MX8M Mini platform.

I am using the ISL79987 Video Decoder.

Do you have an example of how to add ISL79987 to the device tree on the i.MX8M platform?

Best regards.

0 项奖励
回复

1,051 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Benson,

     Sorry for my delay reply!  see below, please!

----------------

In iMX8M internal, the CSI module is used to capture the input camera signal from MIPI CSI2, it can't indetify MIPI virtual channels, so all data will be received in time order line by line. ISL79987 doesn't have buffer in chip, so it can't output whole frame.

 

So I think ISL79987 can't be well supported on iMX8M. To make it work on iMX8M, the ISL79987 need merge the four camera's VSYNC to one, and even in this case, the captured video is still a line combined image. 

----------------

Have a nice day!

TIC weidong sun

1,051 次查看
bruno_chen
Contributor II

Hi, Wigros,

Could you please help me to clarify why the i.MX6DQ could decode ISL79987 perfectly?

Thanks,

Bruno

0 项奖励
回复

1,051 次查看
663831938
Contributor I

Hi, Bruno,

Have you solved this problem? I have encountered the same problem now

 

Thanks,

0 项奖励
回复