Hi NXP.
We are currently having a problem with i.MX6solo's ENET_MDC and are gathering information to resolve it.
Which signal is the clock source for i.MX6solo's ENET_MDC?
I checked the reference manual and can't find any information.
It would be nice if there was documentation showing the connection with PLL.
Best regards.
已解决! 转到解答。
Hi @Ryo_Aoki
It's from enet module clock: ipg_clk, the name in device tree is IMX6SX_CLK_ENET.
It would be nice if there was documentation showing the connection with PLL.
-->I couldn't find such connection diagram
Best Regards
Zhiming
Hi @Ryo_Aoki
It's from enet module clock: ipg_clk, the name in device tree is IMX6SX_CLK_ENET.
It would be nice if there was documentation showing the connection with PLL.
-->I couldn't find such connection diagram
Best Regards
Zhiming
Hi Zhiming.
Thank you for your reply.
However, I am targeting i.MX6solo, not i.MX6SX.
Is the clock source ipg_clk for i.MX6solo as well?
And can the clock source to this ENET_MDC be a different clock source than ipg_clk?
I was assuming that PLL6, for example, was being used.
Best regards.