We're using i.MX8M Plus UART3 for RS-485.
but UART3_CTS_B pin could be driven only 10K MAX. So, it could not be controlled the RS-485 driver device(ADM2587).
Is it the correct behavior?
and, If drive strength set to x6(12mA), it seems to be changed to x2 when MUX set to UART mode automatically.
Hi @MS-MS,
I have included below my comments,
Hi @MS-MS
With reference to the 3.3V Logic level, Vih of 3.3V shall be a minimum of 2V. Since 2.2V is received on the CTS pin, the RS485 driver device shall detect it as high. Could you please confirm if you are facing issues in the communication between the processor and the RS485 device?
Thanks & Regards
Dhruvit Vasavada
Hi @MS-MS
I hope you are doing well
Hi @MS-MS,
I hope you are doing well.
Please remove the R51 resistor to isolate that particular pin and then drive the pin high from the processor. Check if 3.3V is received on that particular pin.
Hi @MS-MS,