i.MX8M Plus UART3 CTS_B drive strength

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Plus UART3 CTS_B drive strength

2,169 Views
MS-MS
Contributor I

We're using i.MX8M Plus UART3 for RS-485.

but UART3_CTS_B pin could be driven only 10K MAX. So, it could not be controlled the RS-485 driver device(ADM2587).

Is it the correct behavior?

 

and, If drive strength set to x6(12mA), it seems to be changed to x2 when MUX set to UART mode automatically.

0 Kudos
Reply
14 Replies

2,141 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MS-MS,

I have included below my comments,

  • Yes, the UART3_CTS_B pin can not be controlled by the RS-485 driver. Rather it is only configured by the Device tree.
  • There is a possibility that the Drive Strength Field(DSE) value could be overwritten by the device tree. Please check the same.
 
 
Thanks & Regards,
Dhruvit.
0 Kudos
Reply

2,120 Views
MS-MS
Contributor I

Thanks,

With your suggestions, It was able to set the drive strength to 12mA.

However, the voltage of CTS_B is up to Hi=2.2V.

0 Kudos
Reply

2,071 Views
MS-MS
Contributor I

I need your additional suggestions.

 

CTS_B Hi-level is not rise to 3.3V.  

Is there any register setting necessary?

 

0 Kudos
Reply

2,064 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MS-MS 

With reference to the 3.3V Logic level, Vih of 3.3V shall be a minimum of 2V. Since 2.2V is received on the CTS pin, the RS485 driver device shall detect it as high. Could you please confirm if you are facing issues in the communication between the processor and the RS485 device?

Thanks & Regards

Dhruvit Vasavada

0 Kudos
Reply

2,062 Views
MS-MS
Contributor I

Thanks,

I'm not sure, why high level of TX/RX are 3.3V but only CTS_B is 2.2V.

Is there different buffer between TX/RX and CTS_B?

 

0 Kudos
Reply

2,046 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MS-MS,

 

I understand your concern. Could you please share the end-to-end schematic connections of the pins used for the RS-485 interface?

0 Kudos
Reply

2,040 Views
MS-MS
Contributor I

Attached please find the schematics.

Thanks.

0 Kudos
Reply

2,027 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MS-MS 

I hope you are doing well

The attached image seems to be a block diagram rather than a schematic. Could you please share the schematic which has the electrical connections with passive components as well?
 
Thanks & Regards
Dhruvit Vasavada

0 Kudos
Reply

2,018 Views
MS-MS
Contributor I

ok. attached.

0 Kudos
Reply

1,991 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MS-MS,

I hope you are doing well.

Please remove the R51 resistor to isolate that particular pin and then drive the pin high from the processor. Check if 3.3V is received on that particular pin.

Thanks & Regards,
Dhruvit.
0 Kudos
Reply

1,988 Views
MS-MS
Contributor I

In such case, CTS_B Hi=2.7V.

0 Kudos
Reply

1,931 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MS-MS,

I hope you are doing well.
 
Kindly set the configuration as given below(default in BSP version 5.15.71) in the device tree and check if the issue is resolved or not. 
If not please check from where the voltage is leaking. Is this pin connected somewhere else also?
As we are getting the 3.3 V on the same pin in EVK.
 
pad 0x30330318=0x10
 
Thanks & Regards,
Dhruvit Vasavada.

0 Kudos
Reply

1,873 Views
MS-MS
Contributor I

If 0x30330318 set to 0x10, there is no change (Still 2.4V)

CTS_B is also connected to GPIO4_IO[9] as default setting(Input).

0 Kudos
Reply

1,851 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MS-MS,

I hope you are doing well

Kindly try after connecting the R51 and removing the R57 resistor. And please measure the voltage at TP23.

 

Thanks & Regards,
Dhruvit Vasavada

0 Kudos
Reply