i.MX8M Plus PCIe M.2 Key support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Plus PCIe M.2 Key support

Jump to solution
1,775 Views
zc_tee
Contributor III

Hi all,

May i know for i.MX8MPlus PCIe, does it support all M.2 module Key A,B,E and M? The eval kit uses Key.E, but we would like to explore if it can do more.

zc_tee_0-1600233288211.png

 

Thank you.
Regards,

Tee

0 Kudos
1 Solution
1,741 Views
art
NXP Employee
NXP Employee

I mean that the i.MX8MPlus processor doesn't have a built-in SATA controller. To support SATA, an external controler, e.g. PCIe-to-SATA controller, should be used.

Best Regards,

Artur

View solution in original post

3 Replies
1,754 Views
zc_tee
Contributor III

Hi @art ,

Thank you for your reply. You mentioned i.MX8MPlus processor does not directly support SATA. What is the meaning of not directly support? What we need to do to make it support SATA?

Thank you.

Regards,

Tee

0 Kudos
1,742 Views
art
NXP Employee
NXP Employee

I mean that the i.MX8MPlus processor doesn't have a built-in SATA controller. To support SATA, an external controler, e.g. PCIe-to-SATA controller, should be used.

Best Regards,

Artur

1,762 Views
art
NXP Employee
NXP Employee

The E specification of the M.2 connector is most optimal for the i.MX8MPlus processor with regard to type and number of interfaces supported. For example, the i.MX8MPlus processor does not directly support SATA, UIM, HSIC, SSIC, and SMBus interfaces and cannot provide 4xDP interfaces.

Best Regards,
Artur

0 Kudos