i.MX8M Plus - GP Timers not connected to the IO pins?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Plus - GP Timers not connected to the IO pins?

Jump to solution
990 Views
erling
Contributor III

Hi all.

I am looking at the Reference Manual for i.MX8M Plus to see if it satisfies my requirements. But I find it very hard to figure out if the peripherals listed in the Specs are actually usable.

E.g. it is written that this SoC has 6 General Purpose Timers, each with 2xInput Capture and 3x Output Compare. However when I am looking at the IOMUX reference it seems as if it is only GPT1 which actually has its Input Capture routed to the IO Pins, leaving GPT2-6 useless wrt Input Capture.

Have I misunderstood something here? It seems a bit odd that I have to dig so much to find out if the listed peripherals actually are functional or not?

Thanks for any advice

Tags (2)
0 Kudos
1 Solution
979 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erling

 

your understanding is correct: only GPT1 has its Input Capture routed to the IO Pins.

 

Best regards
igor

View solution in original post

1 Reply
980 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erling

 

your understanding is correct: only GPT1 has its Input Capture routed to the IO Pins.

 

Best regards
igor