Hi,
We observed the degradation of performance of NNStreamer on i.MX8M PLUS EVK between 2 Yocto Linux version: LF_v5.15.32-2.0.0_images_IMX8MPEVK and LF_v6.1.22-2.0.0_images_IMX8MPEVK.
Test Setup:
NNStreamer run from NXP Demo Experience - Object Detection, with following settings:
Result for v5.15.32-2.0.0:
Result for v6.1.22-2.0.0:
Notice that the FPS has decreased from 5 fps to 2.5 fps.
Please advise why is there a degradation of NNStreamer performance? What can we do to resolve this?
Hello,
I was trying to replicate the issue from my side when I realized that it was very strange to get 5-7 FPS performance if you are using the NPU. When you use the NPU, you should expect performance above 30 FPS. The problem is that this example application does not support webcams. You can try using the OS08A20 camera and you should see better performance. Let me know if this is not the case.
Regards