Hi NXP,
On the i.MX8M EVK, there is an on-board WiFi module. The EVK board has provision for connecting the PCM interface of the WiFi module to the SAI interface of the i.MX8M SoC.
I would like to try the SAI interface with BlueZ HSP profile with this SAI interface. I was wondering what would I need to do to enable the SAI interface for SCO audio connection, other than adding jumper wires for the PCM connection on the EVK board.
On the BlueZ side, what do I need to do so that the BlueZ would know to use the SAI interface for SCO audio?
Thank you so much,
Dawei
Hi Diego,
I have not tried the Bluetooth radio (QCA6174) on the NXP i.MX8MQ platform.
I have tested QCA9377-3 BT on a custom i.MX8MQ platform with the "hciattach" command.
The BlueZ package needs to be patched to support either QCA6174 or QCA9377-3.
For the QCA9377-3 command, I would use the following command. (BT i/f is UART)
hciattach -s 115200 /dev/ttymxc4 qca 4000000 flow nosleep
For QCA6174 PCI-E, I think the BT i/f is USB. I'll check if the same command is applicable.
Are you familiar with the QCA9377-3 Bluetooth on the NXP i.MX8M mini platform?
Thanks,
dawei
Hello,
The i.MX8MM-EVK uses the QCA9377. The command that I use is similar to the one that you use.
# hciattach /dev/ttymxc2 qca 3000000 flow -b -t 120
I did not have any problem with the Audio over a Bluetooth speaker using that command.
Best regards,
Diego.
Hi Deigo,
Could we use the i.MX8MM-EVK as the reference platform and continue with the original questions?
This way you and I could stay original topic. Thoughts?
FYI - the original question is on SCO (Headset profile). A2DP does not use SCO connection.
Thank you so much for the patience.
dawei
Hello,
Unfortunately, this problem is more related to Bluez. Bluez 5.0 does not support the HSP Bluetooth profile. Right now the only supported profile is A2DP. I apologize for the inconvenience this could give you.
Best regards,
Diego.
Hello,
I apologize for the delay this is taking I am facing some problems implementing the Audio over classic Bluetooth. I have this problem escalated internally. I will update you as soon as I have an update.
Best regards,
Diego.
Note to anyone trying to make use of SCO over UART for the Handsfree BT profile with QCA9377 -- it's not supported by Qualcomm. This should have been solved years ago, but still isn't. And it has nothing to do with Bluez. Push you vendor to get Qualcomm/Silex or whoever the integrator is to get this resolved.
Thanks