In continuation with thread,
https://community.nxp.com/message/1313545?commentID=1313545&et=watches.email.thread#comment-1313545
I have a separate question as below:
1) FlexSPI Parallel Mode is for Octal Flash right? Correct me if i am having wrong understanding.
2) Was not able to find the boot configuration changes that has to be done to change the boot from eMMC to QSPI and QSPI Flash to Octal Flash.
Didn't got details to change the boot configuration from QSPI Flash to Octal Flash or vice-versa. Can you please provide some example or reference for the same.
Hi Bimal
>1) FlexSPI Parallel Mode is for Octal Flash right?
right.
2) Was not able to find the boot configuration changes that has to be done to change the
>boot from eMMC to QSPI and QSPI Flash to Octal Flash.
please refer to Table 5-15. Expansion Device eFUSE Configuration,
sect.5.8.3 FlexSPI serial flash memory boot
i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual
>Didn't got details to change the boot configuration from QSPI Flash to Octal Flash or vice-versa.
>Can you please provide some example or reference for the same.
example was sent via mail.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------