i.MX8 Quad Max impedance of PCIE and SATA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 Quad Max impedance of PCIE and SATA

Jump to solution
2,075 Views
anon-696f160ab2
Senior Contributor I

For i.MX8 Quad Max there is only one pin for setting the impedance of PCIE and SATA: PCIE_REXT

 

As SATA and PCIE using different differential impedance i think there is no "optimum" for the impedance.

 

What is the recommendation for PCIE_REXT when using two PCIE-Lanes and one SATA.?

Can we use 85 Ohm for driver but routing with 100 Ohm from SATA specification?

0 Kudos
Reply
1 Solution
1,838 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

preliminary document with routing recommendations was sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
1,836 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,839 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

preliminary document with routing recommendations was sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,838 Views
anon-696f160ab2
Senior Contributor I

Thanks igor, I answered your email, as it wasnt helpful at the moment.

0 Kudos
Reply
1,838 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

this part is not officially released yet and not supported. Suggest to

apply to nxp local marketing office for additional support.

Best regards
igor

0 Kudos
Reply
1,838 Views
RossMcLuckie
NXP Employee
NXP Employee

For the case of PCIe plus SATA use 85-ohm value, BSP SATA driver adjusts PHY register to compensate.

Regards

Ross

0 Kudos
Reply