i.MX8 FreeRTOS on Core M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 FreeRTOS on Core M4

2,518 Views
luca_corna
Contributor I

We are using the A core for main application running on Android. On the M4 Core we would like to put FreeRTOS but I don't find the ported version and any guide. Anybody that can explain me if it exists or not or how to adapt FreeRTOS for this core? I am new in RTOS.

0 Kudos
3 Replies

1,468 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Luca,
The FreeRTOS release for M4 core of i.MX8 is part of the MCUXpresso SDK, which could be build and downloaded (including its related documentation) from the following site:

https://mcuxpresso.nxp.com/en/select 


In case of having doubts regarding how to generate your SDK package, you could refer to the following Community document:
Generating a downloadable MCUXpresso SDK v.2 package 


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos

1,468 Views
luca_corna
Contributor I

Hallo,

I saw that MCUxpresso SDK is not available for my processor. How can I use

the GCC SDK for another IDE (or for MCUxpresso)?

Il giorno gio 7 mar 2019 alle ore 17:13 CarlosCasillas <

admin@community.nxp.com> ha scritto:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: i.MX8 FreeRTOS on Core M4

reply from CarlosCasillas

<https://community.nxp.com/people/CarlosCasillas?et=watches.email.thread>

in i.MX Processors - View the full discussion

<https://community.nxp.com/message/1121947?commentID=1121947&et=watches.email.thread#comment-1121947>

0 Kudos

1,468 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Luca,

I’m afraid that there are no plans to include MCUXpresso IDE as part of the supported IDEs for the MCUXpresso SDK. Just IAR and GCC are supported, as listed on the Release Notes.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos