i.MX7D peripheral pins different power groups?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7D peripheral pins different power groups?

518件の閲覧回数
thomaskofoedhan
Contributor III

I'm trying to configure the pin muxing using the Pins tool, but I keep getting peripherals with pins from different power groups. This makes it very hard to control which banks should be which voltage. Even the keypad pins which I'm working on at the moment can not all come from the same power bank. Is this correct or is there an error in the tool?

ラベル(1)
0 件の賞賛
返信
1 返信

434件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

   This is correct - some signals for modules, say for keypad, may be powered via different
power domains.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信