i.MX7D U-Boot not seeing ENET

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7D U-Boot not seeing ENET

826件の閲覧回数
jtheath
Contributor II

Bringing up a new i.MX7D-based board.  U-Boot doesn't see any FEC MXC ENET interfaces.  Using LAN8710ai.

According to the board designer the ENET1 hardware and configuration closely resembles the mx7dsabresd.  I am admittedly inexperienced with this bring-up task.  What should I be looking for?

 

Attached is a capture of the boot output; board files and modified fec_mxc.c (only fecmxc_initialize_multi() modified to dump phy search results).  Performing "mii info" after interrupting boot displays "NULL device name!  No such device: <NULL>"

 

Thank you,   Joe

Original Attachment has been moved to: mx7d_rpc472.c.zip

Original Attachment has been moved to: mx7d_rpc472.h.zip

Original Attachment has been moved to: fec_mxc.c.zip

ラベル(1)
タグ(2)
0 件の賞賛
1 返信

437件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Joseph

LAN8710ai is rmii while mx7dsabresd uses rgmii on board, it can not be reused directly

Schematics (2)
Design files for i.MX 7Dual (REV D)
Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 7Dual (REV D)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

please check below link for correct rmii connections

RMII interface on the IMX7 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛