Hello,
I am currently planning a hardware design using an i.MX7. Our customer would like to use both NAND and eMMC flash (to strictly split boot and data files).
The plan was to use SD3/SAI1 in alternate pin mux 1 to provide the NAND interface and SD1 to connect to the eMMC.
However, SD1 seems to not have a strobe signal.
Is it possible to use both eMMC (v5) and NAND at the same time?
(From what i have seen, the strobe signal is only used in HS400 mode. In this case, i could use any eMMC in HS200 mode?)
解決済! 解決策の投稿を見る。
Hi Lars
you are right, strobe signal is optional signal used in HS400 mode.
One can use any eMMC in other modes.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Lars
you are right, strobe signal is optional signal used in HS400 mode.
One can use any eMMC in other modes.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------