i.MX7 can't capture high resolution picture base on OV5640 MIPI camera ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 can't capture high resolution picture base on OV5640 MIPI camera ?

721 Views
Danube
Contributor IV

Hi

CPU : i.MX7D

Kernel Version

Yocto_4.1.15_2.0.0

Issue

test the OV5640 camera on i.mx7, it always hangs when it captures the picture with the resolution higher than 640x480.

command :

gst-launch-1.0 imxv4l2src device=/dev/video1 num_buffers=1 ! video/x-raw,format=YUY2,width=1920,height=1080,framerate=30/1  ! jpegenc quality=100 idct-method=2 ! filesink location=test.jpg

Gstreamer log

 

0:00:01.797284750   861  0x1146000 INFO                 imxv4l2 gstimxv4l2.c:902:gst_imx_v4l2capture_config_usb_camera: capture mode 3: 1920x1080
0:00:02.481041750   861  0x1146000 INFO                 imxv4l2 gstimxv4l2.c:914:gst_imx_v4l2capture_config_usb_camera: frame format: YUYV
0:00:02.481155625   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1563:gst_imx_v4l2_set_buffer_count: requeset for (6) buffers.
0:00:02.504577125   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1606:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x1153298), type(1), memblk(0x11565ac), paddr((nil)), size(4147200).
0:00:02.504891375   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1638:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x1153298), type(1), index(0), memblk(0x11565ac), vaddr(0x74f0b000), paddr(0xae100000), size(4147200).
0:00:02.505212375   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1606:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x11532e8), type(1), memblk(0x115665c), paddr(0x3f5000), size(4147200).
0:00:02.505393375   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1638:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x11532e8), type(1), index(1), memblk(0x115665c), vaddr(0x74b16000), paddr(0xae500000), size(4147200).
0:00:02.505492625   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1606:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x1153338), type(1), memblk(0x115670c), paddr(0x7ea000), size(4147200).
0:00:02.505659500   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1638:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x1153338), type(1), index(2), memblk(0x115670c), vaddr(0x74721000), paddr(0xaed00000), size(4147200).
0:00:02.505756125   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1606:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x1153388), type(1), memblk(0x11567bc), paddr(0xbdf000), size(4147200).
0:00:02.505920750   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1638:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x1153388), type(1), index(3), memblk(0x11567bc), vaddr(0x7432c000), paddr(0xaf100000), size(4147200).
0:00:02.506017500   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1606:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x11533d8), type(1), memblk(0x75d018ac), paddr(0xfd4000), size(4147200).
0:00:02.506182500   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1638:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x11533d8), type(1), index(4), memblk(0x75d018ac), vaddr(0x73f37000), paddr(0xaf500000), size(4147200).
0:00:02.506278375   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1606:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x1153428), type(1), memblk(0x75d0195c), paddr(0x13c9000), size(4147200).
0:00:02.506445625   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1638:gst_imx_v4l2_allocate_buffer: Allocated v4l2buffer(0x1153428), type(1), index(5), memblk(0x75d0195c), vaddr(0x73b42000), paddr(0xaf900000), size(4147200).
0:00:02.506587500   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1835:gst_imx_v4l2_queue_gstbuffer: queue gstbuffer(0x75d14850).
0:00:02.506645625   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1748:gst_imx_v4l2_queue_v4l2memblk: queue v4lbuffer memblk (0x11565ac), paddr(0xae100000), index(0), flags(0).
0:00:02.506709500   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1769:gst_imx_v4l2_queue_v4l2memblk: streamon count (2), queue count (0)
0:00:02.506769250   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1835:gst_imx_v4l2_queue_gstbuffer: queue gstbuffer(0x75d148f0).
0:00:02.506817625   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1748:gst_imx_v4l2_queue_v4l2memblk: queue v4lbuffer memblk (0x115665c), paddr(0xae500000), index(1), flags(0).
0:00:02.506879625   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1769:gst_imx_v4l2_queue_v4l2memblk: streamon count (2), queue count (1)
0:00:02.861754875   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1789:gst_imx_v4l2_queue_v4l2memblk: V4L2 device is STREAMON.
0:00:02.861885125   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1835:gst_imx_v4l2_queue_gstbuffer: queue gstbuffer(0x75d14990).
0:00:02.861951250   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1748:gst_imx_v4l2_queue_v4l2memblk: queue v4lbuffer memblk (0x115670c), paddr(0xaed00000), index(2), flags(0).
0:00:02.862041875   861  0x1146000 DEBUG                imxv4l2 gstimxv4l2.c:1800:gst_imx_v4l2_queue_v4l2memblk: queued (3)   ----------> hangs here.

Does any ideas or suggestions how i fix this problem ?

0 Kudos
2 Replies

448 Views
Danube
Contributor IV

Wigros,

I think i.MX7D can process  S/W jpeg encode function base on Gstreamer plug in lib

We are some confuse ,640x480 can work , 

800x600 , 1024x768 fail

Apollo Chang

0 Kudos

448 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Apollo,

    There is no VPU( Hardware encoder) in i.MX7D, so High resolution JPEG encoding can't be supported.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos