Hello together,
i would like to setup my custom board, to boot from eMMC.
In uBoot I found the fuse command.
What bank/word I have to write to access the boot_cfg[1/2/4]?
In ref manual 35.3.2 Fuse Shadow Memory Footprint I see 3 times boot_cfg at addr 0x05 to 0x07.
Does that mean bank 0 word 5/6/7 for boot_cfg[1/2/4]?
If yes, are bit 0 to 7 from boot_cfg[1] are found at bank 0 word 5 bit 0 to 7?
Greetings, Hans
Solved! Go to Solution.
@ Victor & Yuri,
thanks for your reply. I found the glue between u-boot fuse command (with banks and words), the addresses in chapter 5-1 and the position in the OTP-Area.
Greetings, Hans
Please refer table 5-1 "Boot Device Select" in chapter 5 of the Reference Manual.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------