i.MX6solo MAPSR register Should bit16 be set?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6solo MAPSR register Should bit16 be set?

ソリューションへジャンプ
448件の閲覧回数
Ryo_Aoki
Contributor III

Hi NXP.
I have a question about the i.MX6 solo's MAPSR register.
Looking at the register details in 45.12.17, the reset value of bit16 is 0.
Therefore, I think it is appropriate to set bit 16 to 0 when writing to the MAPSR register.

However, as shown below, in the document, 1 is set when writing to the MAPSR register.

ex1) 45.8 LPDDR2 Refresh Rate Update and Timing Derating
1. Set MAPSR to 0x00010107
5. Write MAPSR to 0x00010106 to re-enable this feature

 

ex2) i.MX6DL Register Programming Aids
Ryo_Aoki_0-1702862348355.png

In the Excel file, 1 is written as a fixed value to bit 16 of the MAPSR register.

Should bit16 be set to 1 when writing to the MAPSR register?
I would like to know the recommended value to write to bit16.

Best regards.

 

ラベル(1)
0 件の賞賛
返信
1 解決策
420件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

For the 19–16 This field is reserved. So for the bit 16 you can use the value in the

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
421件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

For the 19–16 This field is reserved. So for the bit 16 you can use the value in the

0 件の賞賛
返信